2012-04-04 4:55 AM
Hello,
I want to use DP83848CVV as Ethenet PHY with STM32F207ZET6 in RMII mode. In Schematics (STM3220G_EVAL),there is some resistor of 51 Ohm in between of signals (RMII_REF_CLK,RMII_TX_EN,RMII_TX_D0,RMII_TX_D1,RMII_CRS_DV) connecting Ethernet PHY & STM32. Are they mandatory?? Please share if any body having any idea. Thanks In advance Regards Balmukund Prasad2012-04-05 4:20 AM
Hello,
For RMII mode, user have to provide the 50 MHz clock by soldering a 50 MHz oscillator (ref SM7745HEV-50.0M or equivalent) on the U3 footprint located under CN3 and also removing jumper on JP5. This oscillator is not provided with the board. For more details, please refer to STM3220G-EVAL evaluation board User manual (UM1057).We’re moving the ST Community to a new platform to give you a better and more reliable community experience.