2012-05-24 1:56 AM
Hi,
I'm using the emdedded stm32l lcd driver on the stm32L152V8t6 (lqfp 100pin) all segments work well,but on the pb4-lcdseg8 I see a fixed voltage level(about 2.9V) very near to the vdd voltage. the lcd glass is ok. or the stm32l152v8t6 has the pb4-lcdseg8 driver broken or there is an error on the datasheet. Can someone confirm me that this pin is working as lcd seg driver ? the following is the port initialization:/* GPIO PB4 LCDSEG8 */
GPIO_InitStructure.
GPIO_Pin
= GPIO_Pin_4;
GPIO_InitStructure.GPIO_Mode
=
GPIO_Mode_AF
;
GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOB, GPIO_PinSource4,GPIO_AF_LCD) ; Thanks in advance2012-05-24 2:26 AM
Probably more dependent on the board, on the STM32L152-EVAL it is jumpered either between the JTAG and LDR via JP10
I'll take a peek at the jumper if I get a chance.RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource4, GPIO_AF_LCD);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOB, &GPIO_InitStructure);
2012-05-24 2:47 AM
Good morning Mr. Clive1,
Thanks in advance for the fast reply.I'm using an empty prototype board without connections on the gpio pins. I tried also to configure the port as input pu-pd or output pp-od,I moved the output state high or low, but I always see about 2.9V. I will try to use another free segment driver or I will replace the mcu.may be that this port is broken(I agree,strange but possible) I don't think that is an issue related to an old library release that I'm using (1.0.0) I hope. regards, spectre2012-05-24 3:39 AM
I don't think that is an issue related to an old library release that I'm using (1.0.0) I hope.
Merging to V1.1.1 wouldn't take much time would it? A quick diff would at least highlight if much had changed
2012-05-24 4:29 AM
I did a comparison on the gpio.c and on the gpio.h,I don't see differences for the package I'm using.So I'll replace the mcu with a working one.
regards spectre2012-06-15 5:28 AM
Yes, I confirm you that it was a faulty(damaged) gpio port :)
regards SpectreWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.