STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HSI and GPS interference

Posted on June 28, 2012 at 01:33 Hello everyone, Did anyone notice that STM32 with an internal HSI at 8MHz cannot be used in proximity to an embedded GPS antenna? The 8MHz internal oscillator happens to have the 197th harmonic close to L1...

michele77 by Associate II
  • 1847 Views
  • 3 replies
  • 0 kudos

Timer Preload and Shadow registers

Posted on June 28, 2012 at 12:38Hi, I am trying to get a better understanding of the timer hardware for the advance control timers. In section 14.3.1 of RM0008 (Rev. 14) it states:- ''The auto-reload register is preloaded.Writing to it or reading fr...

dsjnews by Associate III
  • 3154 Views
  • 4 replies
  • 1 kudos

STM32F107VC CAN bus pin remap

Posted on June 20, 2012 at 23:19hi.i am using the STM32F107VC board from IAR i have some example code for CAN but in my Board they used the PD0 and PD1 for CAN i dont know how to remap it in my code. i have 2 board and i want to sent data between 2 ...

hello by Associate II
  • 5808 Views
  • 20 replies
  • 0 kudos

Max data speed into STM32F4 Discovery via the STLink/V2

Posted on June 27, 2012 at 01:07I was looking to use the STM32F4 Discovery board as an output device which requires a significant bandwidth from the supporting PC.  I don't have specifics nailed down on this task, 115.2Kbaud might be sufficient but ...

dannym by Associate III
  • 3255 Views
  • 5 replies
  • 0 kudos

SDIO can't read more than 511 blocks

Posted on June 26, 2012 at 22:41I'm using the standard STM libaries. I'm using SDIO with DMA. It works perfectly when reading up to 511 blocks but as soon as I try and read 512 blocks it stops working. It would successfully transfer 511 blocks then ...

UART4 interrupts during emulation break

Posted on June 27, 2012 at 11:19Hi, I am using the Keil ARM MDK development tool with an STM32F103ZG microcontroller and ULINK Pro JTAG. I have some UART code that I would like to test which requires the generation of UART transmit and receive inter...

dsjnews by Associate III
  • 2040 Views
  • 4 replies
  • 0 kudos

how to use STM324xG-EVAL projects on STM32F4 discovery board

Posted on June 09, 2012 at 20:15how to use STM324xG-EVAL projects on STM32F4 discovery board????friends i am new to discovery board...nd i want to use SDIO of discovery....bt example progrms for discovry doesnt contain SDIO program bt for STM324xG-E...

rishi by Associate II
  • 2165 Views
  • 4 replies
  • 0 kudos

How to disable the write buffer(ACTLR ,DISDEFWBUF)

Posted on June 27, 2012 at 13:16Basically my application goes into the hard fault handler(where the IMPRECISERR bit is set) and I have read up about this on some forums and found out that I cannot find out the exact instruction causing this fault Ho...

notation

Posted on June 27, 2012 at 14:51Whats the difference about NVIC_SetPriority(TIMER0_IRQn, ((0x01<<3)|0x01)); and NVIC_SetPriority(TIMER0_IRQn, 9);   Is There a special motive to use the first form?????? THANKS #notation

esiqueira by Associate II
  • 1179 Views
  • 2 replies
  • 0 kudos

USB, DMA, CDC and Speed ... Is it possible?

Posted on June 25, 2012 at 23:05Hi all, I have a fair bit of experience with the STM32 now and have got most peripherals working as I want on multiple projects but I am yet to master the USB. I would like to transfer data collected by a series of ...

gareth2 by Associate II
  • 1419 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.