STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32VLDISCOVERY GPIOTOGGLE

Posted on July 01, 2012 at 00:01Hi all, i used pubblic code of GPIOTOGGLE taken from ST site, i try to modify it for toggles led when user button was pressed. i used this modify to main.c  STM32vldiscovery_PBInit(BUTTON_USER,BUTTON_MODE_GPIO);   whi...

Restart from SRAM after Bootloader with problems

Posted on June 30, 2012 at 09:40Hi guys, i managed to flash my stm32f107vc via the internal bootloader, but i have problems to get the program running after it. When I reset the MCU the PC is somewhere at the beginning of SRAM i think (0x20000000)....

STM32F2 USART IDLE Detection

Posted on June 30, 2012 at 15:22Hello,I'am using two STM32F207IG with the UART1's configured as RS232 (8n1,115200, no flowcontrol, asynch) connected via null-modem.Each 10 �s the master sends a byte to the slave (status bit USART_SR_TC is set).My pr...

holger by Associate II
  • 2329 Views
  • 3 replies
  • 0 kudos

Global Triggered timer.

Posted on June 27, 2012 at 11:42Hi All,i am using IAR KickStart Kit for STM32F107VC i have 3 of this board and i am trying to setup like one board will be master and two boards will be slave. the master board should send signal to the slave at exact...

hello by Associate II
  • 3541 Views
  • 7 replies
  • 0 kudos

USART1 simple use problem

Posted on June 29, 2012 at 10:24Hello everybody, I begin with CortexM4 STM32F4 on a keil developpement board (MCBSTM32F400) I try to use USART1 in a very simple mode. I take a look to example and discuss forums. My config seems to be good but no sig...

Beginner with ADC3_DMA, ADC3ConvertedValue constant

Posted on June 28, 2012 at 01:21using gcc 4.5.2, st-util 4242, stm32f4discovery, ADC3_DMA peripheral examples from STM32F4-Discovery_FW_V1.1.0, ld file from TrueStudio, startup file from CMSIS. When I run the program in the debugger the ADC value do...

STM32F4 TIM1 PWM missing ch1..3

Posted on June 28, 2012 at 17:48 STM32F4 TIMER 1 PWM1. Please can someone tell me how to enable channels 1, 2 and 3. Channel 4 is fine generating a PWM at 0..100% at 20Hz. I know channels 1..3 hardware is different - just can't figure out what t...

John F. by Senior
  • 1591 Views
  • 3 replies
  • 0 kudos

PWM on PB.10 and PB.11 with DMA and TIMER2(CH3 e CH4)

Posted on June 28, 2012 at 19:38How can I configure PWM on TIMER2 (CH3 and CH4)? I would like to configure CH4 in other Channel of the DMA, but looks that only run on Channel 2. /* Configuracoes DMA */  DMA_DeInit(DMA1_Channel2);  DMA_InitStructure....

esiqueira by Associate II
  • 1307 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.