2012-06-26 1:41 PM
I'm using the standard STM libaries. I'm using SDIO with DMA. It works perfectly when reading up to 511 blocks but as soon as I try and read 512 blocks it stops working. It would successfully transfer 511 blocks then stop and become non-responsive. It seems like I must be missing something obvious due to the number of blocks it stops on. I looked at the varaibles used and registers but 512 blocks of 512 bytes doesn't seem like it would overun any of them.
I guess the relevant code is below. Where if
NumberOfBlocks
is above 511 it stops working.SDIO_DataInitStructure.
SDIO_DataTimeOut
= SD_DATATIMEOUT; SDIO_DataInitStructure.SDIO_DataLength
= NumberOfBlocks * BlockSize; SDIO_DataInitStructure.SDIO_DataBlockSize
= (
uint32_t
) 9 << 4; SDIO_DataInitStructure.SDIO_TransferDir
= SDIO_TransferDir_ToSDIO; SDIO_DataInitStructure.SDIO_TransferMode
= SDIO_TransferMode_Block ; SDIO_DataInitStructure.SDIO_DPSM
= SDIO_DPSM_Enable;SDIO_DataConfig
(&SDIO_DataInitStructure);
2012-06-26 2:01 PM
Not really rocket science here, but a quick back of the envelope yields
512 x 512 = 262144 (256KB) DMA length count 16-bit units, max data transfer width 32-bits 65535 * 4 = 262140 The cards might well throw in additional limits. You might be able to handle more by chaining DMA transfers at TC.2012-06-27 11:33 AM
Thanks clive1 I knew it would be fairly obvious once I knew where to look but was looking in the wrong place. I was looking at the SDIO limits rather than DMA. Thanks.
2012-06-27 12:51 PM
Personally I think having 16-bit counters and timers on a 32-bit micro is a bit of a cop-out.
I suppose having ridiculously large DMA transfers could be problematic, the limit should at least be able to act on the entire external memory buffer space.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.