2012-06-27 2:19 AM
Hi,
I am using the Keil ARM MDK development tool with an STM32F103ZG microcontroller and ULINK Pro JTAG. I have some UART code that I would like to test which requires the generation of UART transmit and receive interrupts whilst the emulator has stopped on a code breakpoint. Is there a way to generate transmit or receive interrupts when the emulator has stopped at a breakpoint?2012-06-27 4:42 AM
No, stopping the core is invasive. Things like watchdogs can be stopped or enabled during debug as they are independently clocked peripherals rather than executing code.
If you need real-time diagnostics the cheap route is to instrument your code and output telemetry via another serial port to understand code flow and interaction. The expensive route is to use trace hardware and analyze what has happened. The USART could be serviced by DMA, but that will be limited to the resources you had set up prior to stopping.2012-06-27 5:10 AM
Many thanks!
Jo2012-06-27 11:55 AM
Telemetry via the SWO (Serial Wire Output) port should be possible with the Ulink. That should be less intrusive to your application than using another USART. See ST Technical Note TN0132 [Doc ID 16243] ''STM32 Serial Wire Viewer and ETM capabilities with EWARM 5.40 and MDK-ARM 3.70''.
2012-06-27 12:37 PM
I've tried to make the ITM SWV work on a couple of occasions without much joy, not sure if I have the wrong ULink version or firmware, or if it doesn't work with eval releases. Without an interrupt or a buffer behind it a real serial port is preferable if available.
Link to the mentioned tech noteWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.