Anyone tried Altium Designer TASKING?
Posted on August 11, 2009 at 19:35Anyone tried Altium Designer TASKING?
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on August 11, 2009 at 19:35Anyone tried Altium Designer TASKING?
Posted on July 25, 2012 at 16:23I'm relatively new to the STM32 world and would like to ask a question. Using C what is the fastest method to set/reset a GPIO pin state? Currently I'm using the ''a->BSRRL = b'' type of statement. This generates 4 as...
Posted on July 22, 2012 at 17:00Hello everybody :)I'm a beginner in stm32 discovery programming & I want to use usart but I haven't found any example using this peripheral please can you help me #usart #stm32f1xx
Posted on July 25, 2012 at 01:46Hi, I am cery confuse about how to set DMA parameters. I would like to capture images from camera using DCMI module. I don't understand Burst and BufferSize params of DMA. I would like to capture QCIF (176x14...
Posted on July 22, 2012 at 12:21I have been building my own Boards. And have experience with an assortment of Micros. WARNING #1 : I have found that these STM Chips are Very SENSITIVE to Voltages. I accidentally tied the USB 5V source to the VDD Bus...
Posted on July 24, 2012 at 19:04General Purpose Timer 4 counts the position from incremental encoder in quadratur mode. The Encoder has 200 slots and for low speeds, the frequency is rather low. To derive the rotation speed, I subtract 2 positions i...
Posted on March 07, 2012 at 15:22I configure SPI2 and I2S2_ext for running I2S in fullduplex mode using DMA1_Stream4 and DMA1_Stream2. DMA1_Stream4_IRQHandler called and i2s tx is working fine, but DMA1_Stream2_IRQHandler not called at all. Please ...
Posted on July 16, 2012 at 18:06Hi all!!!Please help me. A have problem with I2S interface in this MC. I need to work with audio codec cs4221 by means of I2S. I setup I2S2 interface in full-duplex mode (I2S2- Master reciev, I2S2ext - Slave TX). Data...
Posted on July 16, 2012 at 11:22Hi, I am new to LCD display controller. I am using Olimex STM32F207 board with onboard 6610 LCD color 128x128 TFT display. I have initialized the LCD according to Example code. I my case I could see LCD backlight is ...
Posted on July 22, 2012 at 03:26Greetings, I have a small number of bytes (less than 80 bytes) that I need to store in persistent storage, but the values may change in excess of 10,000 times. I believe the SRAM would work fine for this, but I would...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.