STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IWDG DBGMCU

Posted on July 02, 2012 at 15:01Hi, I  am using IWDG and it works good. I would like to stop it when core halts (in breakpoints), therefore i did:   DBGMCU->CR |= DBGMCU_CR_DBG_IWDG_STOP; But it does not stop the IWDG. Do i miss something? Thanks.

ybitton by Associate II
  • 1310 Views
  • 1 replies
  • 0 kudos

Programming the STM32F4

Posted on July 17, 2012 at 05:01Hi, I originally was planning on using the Discovery demo board, but have since changed to placing the MCU directly on my PCB. Now what is the easiest way to program the thing? The Discovery uses a STM32F103C8T6, per...

Does anyone have a quick and dirty i2c example?

Posted on November 22, 2011 at 00:18Hi all, I am very new to the STM32, currently using the STM32L.. As I am new to developing on this platform (Never touched anything ARM before), I am overwhelmed by the amount of documentation although trying to ...

STM32F4 and TFT 3.5'' SSD1963

Posted on July 16, 2012 at 10:01Hi all! I connected STM32F4 board to a LCD 3.5'' TFT with SSD1963 driver and FSMC controller. I wrote some code like this:http://www.mediafire.com/download.php?v762hz2pdxxxlz1 but the screen like a TV when I disconnec...

mdphuong by Associate
  • 1906 Views
  • 2 replies
  • 0 kudos

Use Printf for USB

Posted on July 20, 2012 at 15:02 Hello, I need an example on STM32 of how  to use printf to format and output data via USB CDC communication (VCP demo) . Does any one had do it before ? Thanks

gafsos by Associate II
  • 1524 Views
  • 2 replies
  • 0 kudos

STM32F407 - I2S2ext clock must be on PB13...?

Posted on June 04, 2012 at 17:54While working on I2S on STM32F407, I came across an issue I believe is a bug in silicon. I need duplex I2S, so I have configured I2S2 as Master Receiver and I2S2ext as Slave Transmitter, with outputs on port I, i.e. P...

Matlab / Simulink Support for STM32F4Discovery board

Posted on January 07, 2012 at 18:50I have found a presentation about STM32 F4.  On page 45, it says Simulink demo will be released by the end of 2011.. http://catalog.compel.ru/blog/wp-content/uploads/2011/12/3-STM32F4-CM4-High-Performance.pdf Does ...

timurlar by Associate
  • 2698 Views
  • 5 replies
  • 0 kudos

STM32 SPI/I2S and TI ADS7951 ADC

Posted on July 16, 2012 at 17:09Hello everybody,I'm evaluating the STM32F207IG and I need to acquire samples from an ADC from Texas Instruments (ADS7951), which is a 12bit 1MS/s serial ADC.The ADC interface is a sort of SPI, with MISO, clock and a C...

Problems with interupt-configuration

Posted on July 19, 2012 at 15:50 Hello, in my Application I have got a LED which is toggled by Timer2. When only this timer is running, the output level of the I/O pin is 3V when high. When I additionaly activate the USART interrupt,...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.