2012-07-24 4:46 PM
Hi,
I am cery confuse about how to set DMA parameters. I would like to capture images from camera using DCMI module. I don't understand Burst and BufferSize params of DMA. I would like to capture QCIF (176x144) YUV 4:2:2 from a camera to an array buffer. Here is the parameters that I use but it doesn't work.. DMA_InitStructure.DMA_Channel = DMA_Channel_1; DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)DCMI_DR_ADDRESS; DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)frame_buffer; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_BufferSize = (176*144)/4; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; //single register DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; //frame_buffer++; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure.DMA_Mode = DMA_Mode_Normal; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; /* DMA2 IRQ channel Configuration */ DMA_Init(DMA2_Stream1, &DMA_InitStructure); Thanks2012-07-24 4:50 PM
and this is my DCMI config part;
DCMI_InitStructure.DCMI_ExtendedDataMode = DCMI_ExtendedDataMode_8b;//bit[11:10]: 8bit-data/pclk DCMI_InitStructure.DCMI_CaptureRate = DCMI_CaptureRate_All_Frame; //bit[9:8]: Frame Capture Rate Control DCMI_InitStructure.DCMI_VSPolarity = DCMI_VSPolarity_High; //LOW //bit[7]: VSYNC active @low DCMI_InitStructure.DCMI_HSPolarity = DCMI_HSPolarity_Low; //bit[6]: HSYNC active @high DCMI_InitStructure.DCMI_PCKPolarity = DCMI_PCKPolarity_Rising; //bit[5]: PCLK at Rising Edge DCMI_InitStructure.DCMI_SynchroMode = DCMI_SynchroMode_Hardware; //bit[4]: use hardware VSYNC/HSYNC //DCMI_JPEGCmd(ENABLE/DISABLE) bit[3]: JPEG Mode //bit[2]: Crop mode DCMI_InitStructure.DCMI_CaptureMode = DCMI_CaptureMode_Continuous; //bit[1]: //bit[0]: capture 0:disable/1:enable DCMI_Init(&DCMI_InitStructure);2012-07-24 6:13 PM
Here is what I do with my DMA. I am tranfering alot more data per frame.. but this works for me..
/* DMA Stream Configuration */ DMA_DeInit ( DCMI_DMA_STREAM ); DMA_InitStructure.DMA_Channel = DCMI_DMA_CHANNEL; DMA_InitStructure.DMA_PeripheralBaseAddr = DCMI_DR_ADDRESS; DMA_InitStructure.DMA_Memory0BaseAddr = DCMI_IMAGE_SRAM_ADDRESS; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_BufferSize = 0xffff;//Maximum DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_VeryHigh; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init ( DCMI_DMA_STREAM, &DMA_InitStructure ); DMA_DoubleBufferModeConfig(DMA2_Stream1, DCMI_IMAGE_SRAM_ADDRESS + ( 0xffff * 4 ), DMA_Memory_0); DMA_DoubleBufferModeCmd(DMA2_Stream1, ENABLE);I was having issues myself and got some help here on the forums.
Check out these two posts if you interested.https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Some more DCMI problems F207IG&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=452
https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/DCMI Issues, looking for insight&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=1400
Hope this helps! Cheers, Brad2012-07-24 6:31 PM
Thanks Brads :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.