2012-07-21 6:26 PM
Greetings,
I have a small number of bytes (less than 80 bytes) that I need to store in persistent storage, but the values may change in excess of 10,000 times. I believe the SRAM would work fine for this, but I would rather not use the extra battery power to maintain the SRAM if the 80-byte memory in the backup domain can handle the write frequency I anticipate. What kind of memory is this 80-byte user memory? What are the specs for number of writes? Thanks, Valkyrie-MT #sram-backup-rtc2012-07-23 7:02 AM
The backup registers are SRAM powered from the backup (Vbat) power domain. For the STM32F1xx series these are 16-bit half words; don't try to use 32-bit access. You will need a battery or some other backup supply (i.e. supecap) in order to save data in the backup registers. Be aware that a tamper event (if you have it enabled) will erase the 80 byte backup register area.
Jack Peacock2012-07-23 9:28 PM
Excellent! Exactly the answer I was hoping for! And thanks for the tip on the tampering. I'll have to figure out how to disable that.
-Valkyrie-MTWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.