STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f100 Flash Programming strangeness

Posted on August 06, 2012 at 14:38Hi, Now I'm using a stm32f100c4t6b processor for an application. The proccessor has 16KB memory. I saved my data like that;#define StartAddr  ((u32)0x08007C00)#define EndAddr    ((u32)0x08008000)#define FLASH_PAGE_S...

acihana by Associate II
  • 1477 Views
  • 3 replies
  • 0 kudos

Complex FFT

Posted on August 06, 2012 at 12:22Hello, i am working on science project involving fast calculations for laser stabilization. I need to calculate complex FFT and get phase of second maximum in spectra (first will be 1/f noise, second should be right...

linas2 by Associate II
  • 787 Views
  • 0 replies
  • 0 kudos

Issues with RTC

Posted on August 03, 2012 at 10:43 Hi gents, We're using a STM32F217IGH6, in a Silica Xynergy board, and we're experiencing some strange issues with the RTC. The code regarding RTC is: static void rtcConfiguration( void ...

fbenito by Associate
  • 1662 Views
  • 2 replies
  • 0 kudos

STM32F1xx and STM32F2xx HSI stability

Posted on March 13, 2012 at 16:47Hello! I have a question to STM32xx chip manufacturers. Last yar I uses STM32F10xx chips in my applications. It's 8mHz HSI works perfect - stable, with small temperature sensistivity - works very well.  CAN bus (slow...

denlok by Associate II
  • 1759 Views
  • 3 replies
  • 0 kudos

To many elements in the array - stm32f103

Posted on July 27, 2012 at 21:29hello, I have an issue. I'm using the stm32f103RB. When i want to create an array which has 8192 elements - const uint16_t table[8192] = {458,542...  }; The software successfully build in to the flash, but when i'm st...

dzbogar by Associate
  • 1525 Views
  • 3 replies
  • 0 kudos

Driver to use MicroSD card with SPI

Posted on March 07, 2012 at 11:12Hi, I develop a project on the STM32F4 discovery board and I want use a MicroSD card. I work with Atollic TrueStudio for STM32. So I search a driver to use my MicroSD card with SPI. I have an API to FATFs and an API ...

UART stm32f4 discovery

Posted on August 02, 2012 at 13:07Hi , i've a problem, i don't manage the sending of the UART signal in correct manner using  stm32f4 discovery. I've need of the correct procedure to send Uart signal. Every help is accepted. Thank you. #stm32-di...

lacava by Associate II
  • 1685 Views
  • 4 replies
  • 0 kudos

TFT driver INternal memory

Posted on July 31, 2012 at 17:28Hi all, To begin I have compiled AN2790 and AN3241 application note, to try understand logic code. These notes explain how use TFT with firmware ST. I have several questions about it. Is it possible, to display a pict...

erwann by Associate II
  • 2461 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.