STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ILI9325 without fsmc white screen problem

Posted on August 09, 2012 at 21:04Hi, i am using stm32f103rbt6 (a known board model called stm-mini), but i have some problems with this hardware. I am sure the stm is fine the problem is the ILI9325 lcd. First, all worked fine. So i started to load...

jltellop by Associate
  • 822 Views
  • 0 replies
  • 0 kudos

USB3340 from SMSC allways working in FS usin a STM32F407

Posted on August 01, 2012 at 18:11Hi All, I have developed a PCB that contains an USB3340 and a STM32F407, using the: STM32_USB-Host-Device_Lib_V2.1.0. But is allways working as a FS device instead of a HS one. I have tried the same code in the STM3...

angel2 by Associate
  • 1458 Views
  • 2 replies
  • 0 kudos

STM32F4 I2C Issue?

Posted on May 23, 2012 at 18:47At a high level, I'm able to get I2C on the STM32F4-Discovery board working with our part (MAX5418), but there's one problem I'm having, and that is that I have to write commands twice in order for them to be received....

Random code hangs

Posted on August 07, 2012 at 19:42HelloI dont know why, but when I use FFT code, STM32F103RBT6 just stop running in totally different part of code - mostly in parts of STD library where asserts are defined. So I think it can corrupt memory or someth...

zexx86 by Associate II
  • 2373 Views
  • 4 replies
  • 0 kudos

F0 Discovery - fprintf function implementation

Posted on August 02, 2012 at 22:05Wondering if anyone in the forums has made an fprintf function or equivalent?  I got characters spitting out to hyperterminal, now just trying to figure out to spit out variable info to the screen.

wbarkley by Associate II
  • 1492 Views
  • 6 replies
  • 0 kudos

How to escape USART1 interrupt?

Posted on August 06, 2012 at 22:51Below is my USART1 handler: void USART1_IRQHandler(void) {     if(USART_GetITStatus(USART1, USART_IT_RXNE) != RESET){         USART_SendString(USART1, ''\r\n======Blow ME======\r\n'');         USART_ITConfig( USART1...

wbarkley by Associate II
  • 1953 Views
  • 4 replies
  • 0 kudos

Problem:Immediate call to ISR

Posted on August 08, 2012 at 16:31I have used external interrupt 0, 8 and 9. Before enabling the interrupt i have written the following codes: EXTI_ClearITPendingBit(EXTI_Line8); EXTI_ClearITPendingBit(EXTI_Line9); The interrupt is only called by to...

STM32F103ZE USART1 interrupt issue

Posted on August 07, 2012 at 15:13 Hi, I have problem with USART1 interrupt implementation. In pooling mode, everything works, but when I try to setup interrupt, there's nothing on the output? How to enable USART1 interrupt? Do I need ...

dusan by Associate II
  • 1527 Views
  • 4 replies
  • 0 kudos

RTC in millisecond

Posted on August 07, 2012 at 09:38Hello,I implemented the RTC example of ST (calendar, time counter) but it seems to work just with an interval of 1 second. I need it to work with an interval of 1ms. How can I do it?Thank you!Best regards

stm32f407 discovery Uart

Posted on August 04, 2012 at 16:02Hi,   Board:Stm32F407 Discovery(stm32f407vgt6) i play with my discovery using two uarts.They are Uart4 and Uart5. Uart4 is used for receiving the string from  RFid sensor using uart4 interrupt.RFid sensor is grand i...

vinothraj by Associate II
  • 2890 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.