2012-08-06 3:22 AM
Hello, i am working on science project involving fast calculations for laser stabilization.
I need to calculate complex FFT and get phase of second maximum in spectra (first will be 1/f noise, second should be right signal) since i only need to calculate one complex point in frequency domain, what is fastest way to do that ? (idea is to read CCD array, use 16b adc to read data to STM32F4 and make 16/32/64 or 128 point CFFT for one point, and send that value to laser via DAC ) and what kind of speed i should expect ?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.