2012-08-02 7:49 AM
I'm trying to make a custom drive based on MCS driver; In order to run a STM32F4 (on a discovery board) as USB host of a vendor specific device.
Using USBH_BulkSendData I have exchanged data in OUT direction with success;However, with USBH_BulkReceiveData I cannot receive - IN direction;The post linked below indicates that the library has some problems in its USB machine (but for STM32F1);In this case, the programmer also used the USBH_BulkReceiveData fucntion:[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/USBH_BulkReceiveData problem&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=200]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FUSBH_BulkReceiveData%20problem&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=200Is it really? Has ST a perspective to release a corrected version of the library?Have someone used the function USBH_BulkReceiveData??Thanks in advance.2012-08-02 12:22 PM
> However, with USBH_BulkReceiveData I cannot receive - IN direction;
I recommend you to get more clues, before blaming USBH_BulkReceiveData Are you using this function in right way? Does your target device respond to the bulk IN transaction?> The post linked below indicates that the library has some problems in its USB machine (but for STM32F1); The patch on the link implements time out feature (NAK count timeout) to the original ST's code, to cope with a bad-mannered target device, which doesn't terminate transfer with a short packet like ZLP. Of course, time out feature is desirable. But it doesn't concern to your problem.> Have someone used the function USBH_BulkReceiveData??
It is heavily used in USB_Host_Examples\MSC example. You are starting on this example. Why aren't you aware of? Tsuneo
2012-08-02 12:43 PM
It is the point, Tsuneo;
I debugged the STM32 for the MSC example, and I observed that the USBH_BulkReceiveData works perfectly, as all the other functions.Using a sniffer, as you recommended, I observed that my device can perform Bulk transfers with the PC;But here is my problem: Why doens't work when the STM32 is the host?Follows a example of bulk transfer performed between my device and the PC:Request # 84 [IN]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.