2012-08-08 7:31 AM
I have used external interrupt 0, 8 and 9. Before enabling the interrupt i have written the following codes:
EXTI_ClearITPendingBit(EXTI_Line8); EXTI_ClearITPendingBit(EXTI_Line9); The interrupt is only called by toggle switch. For the first time when i run the program, the interrupt service routine is called instantly once. Apart from that everything works well but i could not debug why the interrupt is called immediately once when the program runs. The input are PC8 and PC9 and they are configured as 'floating input mode' I would be happy if someone could help me on this. #interrupt-immediately-calledWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.