STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Understanding USB at Low Level from Host

I am Implementing RNDIS Over USB using the Stack provided by STM32 Team. The Data Received at the EP OUT Function is Correct for the First Few Bytes of Data, Post that the Data is Jumbled/Incorrect. Not Sure whats the Reasons though.I tried Verifying...

Pavan_LohiaGroup_0-1729255535363.png Pavan_LohiaGroup_1-1729255600629.png

STM32WL55JC intermittently fails to wake from shutdown

I have a STM32WL55JC part that spends a lot of time in shutdown mode. It's woken by an alarm on the internal RTC. However intermittently it fails to fully wake up.This is almost certainly a hardware fault - certain PCBs are more susceptible than othe...

Andy_ by Associate
  • 2664 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to Configure STM32H7B0VB for SDRAM

For my current Project, I decided to go with the STM32H7B0VBT6 from the STM32H7B0VB family. However the 1.4MB SRAM of the MCU was too little for me, so I've chosen to go with an external SDRAM (IS42S16400J-7TLI [64 MBit | 8 MB). Now I wanted to get t...

tlgw by Associate
  • 2624 Views
  • 2 replies
  • 1 kudos

USART not working when using HSI in STM32F769-Discovery

Hi, I am new on STM32 and I started a product prototype using STM32F769-Discovery. I developed all software using default clock configuration, which uses HSE. Now I want to change to HSI, but USART is not working ( Not true, only works when board res...

RCres.1 by Associate III
  • 4545 Views
  • 6 replies
  • 2 kudos

Resolved! STM32H562RGT6 RAM address order

Hi,we are examining if we can apply our March-C test to the STM32H562. It is tailored to the RAM address order of the STM32F446. Unfortunately, the documentation does not seem to provide any hints here. Is there a difference in RAM address order betw...

rt33 by Associate
  • 1952 Views
  • 3 replies
  • 0 kudos

MPU on STM32H755

I'm having a hard time figuring out how to configure the MPU of my microcontrollore in order to have this behaviour.I've a framebuffer in ram that is big 384KB. I've modified my linker in order to have the framebuffer starting at location 0x24022000T...

sbi by Associate III
  • 2156 Views
  • 4 replies
  • 0 kudos

MCU is not recognized as USB storage device

Hi all - I'm new to the STM ecosystem and I've been stuck on an STM32H743/ Micropython issue.My (custom) board can upload Micropython firmware via both SWD and DFU. So DM/ DP work.VCC measures 3.21V, maybe a little low, maybe just my DMM.I'm not able...

Sophi by Associate II
  • 3692 Views
  • 6 replies
  • 2 kudos

Resolved! Serial SPI in one slave

I have two MCUs and I connected them by SPI, one of them is master and another is slave.On slave MCU, I used two SPI1 and SPI2 and I connected them serially by wire, sometimes connect and disconnectthem by S1, I want to ask is it possible to have thi...

02-SPI.png 01-SPI.png
Iraj by Associate
  • 3812 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.