2012-09-06 1:49 AM
ello,
I sometimes have problems with blocks which are written completely wrong onto the sd-card. Workaround: actually I check the written data again by reading the same block from SD-card and check the both buffers if they are equal. Now I have problems to get the CRC-check working on my STM32F103 controller. Here is a small dummy-routine:
/*!< Send CMD24 WRITE_SINGLE_BLOCK */
SDIO_CmdInitStructure.SDIO_Argument = WriteAddr;
SDIO_CmdInitStructure.SDIO_CmdIndex = SD_CMD_WRITE_SINGLE_BLOCK;
SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short;
SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No;
SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable;
SDIO_SendCommand(&SDIO_CmdInitStructure);
/* Set the BlockSize and so on */
SDIO_DataInitStructure.SDIO_DataTimeOut = SD_DATATIMEOUT;
SDIO_DataInitStructure.SDIO_DataLength = BlockSize;
SDIO_DataInitStructure.SDIO_DataBlockSize = (uint32_t) 9 << 4;
SDIO_DataInitStructure.SDIO_TransferDir = SDIO_TransferDir_ToCard;
SDIO_DataInitStructure.SDIO_TransferMode = SDIO_TransferMode_Block;
SDIO_DataInitStructure.SDIO_DPSM = SDIO_DPSM_Enable;
SDIO_DataConfig(&SDIO_DataInitStructure);
/* Start DMA transfer */
SDIO_ITConfig(SDIO_IT_CTIMEOUT | SDIO_IT_DTIMEOUT | SDIO_IT_DATAEND | SDIO_IT_TXUNDERR | SDIO_IT_RXOVERR | SDIO_IT_DCRCFAIL | SDIO_IT_CCRCFAIL, ENABLE);
SD_LowLevel_DMA_TxConfig((uint32_t *)writebuff, BlockSize + sizeof(uint16));
SDIO_DMACmd(ENABLE);
So, I transfer one datablock (512 bytes) + a uint16 with containing a dummy-CRC value.
I think this should result in a CRC error, because the dummy CRC value is not correct? But I will get no CRC-error. Do I have to activate the CRC check manually?
The manual says:
“During block write (CMD24 - 27) one or more blocks of data are transferred from the host to
the card with a CRC appended to the end of each block by the host. A card supporting block
write is always able to accept a block of data defined by WRITE_BL_LEN. If the CRC fails,
the card indicates the failure on the SDIO_D line and the transferred data are discarded and
not written, and all further transmitted blocks (in multiple block write mode) are ignored.�
In WaitWriteOperation() I check:
if(SDIO_GetFlagStatus(SDIO_FLAG_CCRCFAIL) || (SDIO_GetFlagStatus(SDIO_FLAG_DCRCFAIL)))
{
TransferError = SD_ERROR;
}
And also the Interrupts SDIO_IT_DCRCFAIL | SDIO_IT_CCRCFAIL will not fire.
What´s wrong here?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.