STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

measure time for a puls with ADC

Posted on August 29, 2012 at 16:40I need to measure the averige a signal is low using the ADC. Is there a way to connet the adc to a timer? I have nott been able to figure that out, so insted I have tried the folowing... Start systick at 1ms, that c...

oe2 by Associate III
  • 2150 Views
  • 6 replies
  • 0 kudos

UART junk values

Posted on September 03, 2012 at 09:20Hello, I was using UART4 pin PA0 and PA1 for my project. I have done all the initialization procedures right but ended up getting junk values at the output. below is my initialization function. void UART_LowLevel...

vivek2 by Associate II
  • 4312 Views
  • 9 replies
  • 0 kudos

Problems with usart comunication with interrupts

Posted on September 03, 2012 at 09:13Hi, I'm trying so hard to send and receive data through USART1 of my STM32. I'm using STM32VL_Discovery board, Modbus as communication bus with RS485 interface (I connect my micro to the bus through a MAX232 and ...

STM32F0 MIPS

Posted on September 03, 2012 at 15:29Hi, How many Million Instructions Per Second The M0?

Resolved! malloc library - _sbrk problem

Posted on September 02, 2012 at 00:47I was trying to use malloc in a project  which has been ported from an other platform. I get the message that... _sbrk  ... is undefined. This is used by _sbrk_r which again is used by malloc. I found no solution...

Zainka by Associate III
  • 1508 Views
  • 2 replies
  • 0 kudos

STM32F4 Bit Set Reset Register

Posted on August 31, 2012 at 12:09 The file stm32f4xx.h defines the BSRR as two 16 bit ''halves''. typedef struct { __IO uint32_t MODER; /*!< GPIO port mode register, Address offset: 0x00 */ __IO uint32_t OTYPER; /*!< GPIO port output...

John F. by Senior
  • 1912 Views
  • 4 replies
  • 0 kudos

Simulating Alternate Function Input

Posted on October 26, 2011 at 20:27In the STM32 reference manual (Doc ID 13902 Rev 13) in section 9.1.4 it states:It is also possible to emulate the AFI input pin by software by programming the GPIO controller. In this case, the port should be confi...

SDIO Wide Bus Enable Issue

Posted on April 11, 2012 at 10:00In my diskio.c wrapper for fatfs file system i have now got the problem of not been able to enable 4bit wide bus on SDIO. Below is the functions i call in disk_initailse().errorstatus = SD_Init();errorstatus = SD_Get...

UM0427 equivalent for STM32Lxx series

Posted on September 03, 2012 at 06:21Hi, Is UM0427 have an updated version for STM32Lxx series? I searched ST site but to no avail. Can anybody point me to where it was located? thanks in advance. g #stm32l-firmware-library #um0427

gmp383 by Associate
  • 698 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.