STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

JTAG debugging issues

Posted on October 10, 2012 at 19:59Hi, I am trying to connect to the STM32F103VBT6 via JTAG. I am using TIAO JTAG controller (similar to OLIMEX) with OpenOCD. JTAG itself seems to work fine. It can read ID correctly. However I can not halt the core....

vadim23 by Associate
  • 1421 Views
  • 1 replies
  • 0 kudos

STM32L151 executing code from internal Ram

Posted on September 23, 2012 at 23:13Are there any examples or application notes about how to  execute a  Code from internal Ram , i need to do IAP , but when programming flash from a flash based code , the controller  hangs and even debugger can't ...

akp25i by Associate II
  • 2769 Views
  • 5 replies
  • 0 kudos

flash write protected

Posted on October 11, 2012 at 09:59Hi,my stm32f205ze controller become write protected,when i am trying to program its flash option bytes i was written all sectors write protect command. now i am unable to load the program now.what i can do to remov...

STM32F0: Getting PWM Output to Work

Posted on October 08, 2012 at 05:20I can get PWM output to work with my F4 MCUs, but I can't get it to work with the F0. My code is below, any ideas? As you can see, I'm not using the STM libraries, I am only using their stm32f0xx.h header for regis...

upgrdman by Associate II
  • 1647 Views
  • 2 replies
  • 0 kudos

Delay() and System Clock in STM32VLDiscovery ?

Posted on October 10, 2012 at 13:37Hi everyone,I'm new with STM's MCU and I'm doing some tests on the the STM32VLDiscovery board (with MCU : STM32F100RB) I've just bought.I wrote a simple code for blinking a LED and tested it successively on the eva...

edgar2 by Associate II
  • 1777 Views
  • 2 replies
  • 0 kudos

Offset error or conversion error?

Posted on October 10, 2012 at 22:00  The original post was too long to process during our migration. Please click on the attachment to read the original post.

orn by Associate II
  • 1241 Views
  • 4 replies
  • 0 kudos

custom bootloader and peripherals in application

Posted on October 06, 2012 at 03:03hello, I am using STM32F107 with custom bootloader. Quite a few peripherals are initialized and used in a booloader. At some seminar (don't remember which one) I asked about reinitializing peripherals after the jum...

Setting up SPI-bus

Posted on April 11, 2011 at 10:56Hey, Im trying to set up an SPI-bus between the STM32VLDISCOVERY and an external flash memory. I want the STM32-processor to be master and the flash-memory to be slave. What ive tried to far is simply to set up the G...

reckan by Associate II
  • 1687 Views
  • 4 replies
  • 0 kudos

PDM Filter

Posted on April 24, 2012 at 00:01Hi. If  i want to use PDM_Filter_64_LSB() function from pmd_filter.h in my program or just build the ''Audio_playback_and_record'' project, i got a 'undefined reference to PDM_Filter_64_LSB' error. I guess i have to ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.