STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L151 Flash write speed

Posted on October 12, 2012 at 15:35Hello all, I have a question about in application programming speeds with the L151. I have a working bootloader for both the L151 and the F207 micros. They are nearly 100% identical take a master/slave setup. For i...

stbbrad3 by Associate II
  • 2749 Views
  • 2 replies
  • 0 kudos

Missing Cortex-M3 instruction timing

Posted on October 11, 2012 at 10:00ST Cortex-M3 programming manual nicely describes all instruction, how they work and what they do but there is no info how many clock cycles it takes to execute given instruction.Fortunately I found ARM Cortex-M3 ma...

zzdz2 by Associate II
  • 2372 Views
  • 5 replies
  • 0 kudos

compensating networks

Posted on October 11, 2012 at 22:08Is there a library that implements compensation networks such as PID for STM32F4xx? #compensating-networks-pid

betuel by Associate II
  • 1797 Views
  • 3 replies
  • 0 kudos

STM32F4-Discovery - USART problem

Posted on October 09, 2012 at 23:15Hi, I'm trying to connect together two USARTs. First is set as a transmitter and second as a receiver. I connect together two pins on the board PA9 - USART1_TX and PC7 USART6_RX. I have problem with receving data b...

bkdi by Associate II
  • 2947 Views
  • 7 replies
  • 0 kudos

TIM1 to TIM3 PWM

Posted on October 11, 2012 at 09:48Good morning, i'm working with a stm32F0-Discovery board (cortex M0), i need to change the PWM pin from PA8 (using TIM1) to PC8 (using TIM3), but there is a problem because it works wrong.In the following codes i h...

pietro2 by Associate II
  • 1527 Views
  • 2 replies
  • 0 kudos

SPI and Ethernet Controller 28j60

Posted on December 02, 2011 at 06:03Hi everyone,I'm starting with the stm32f100rb and trying to set up the communication with 28j60(SPI). As far as know the 28j60 only support the spi mode 0 and  run at frequencies of at least  8 MHz.To compile with...

sampling frequency

Posted on October 11, 2012 at 09:31Hi everyone!I'm new to the world of microcontrollers. After some research, I bought my first ARM based Microcontroller; the STM32F4 Discovery.Now, I have a few questions for the community, hopefully someone can ans...

betuel by Associate II
  • 1538 Views
  • 2 replies
  • 0 kudos

Alternate Function Input on STM32F4

Posted on September 22, 2012 at 03:30I'm familiar with using alternate function inputs on the STM32F1 series; the associated GPIO pin is set as an input (CNFx[1:0], MODEx[1:0] bits), AFIO clock is enabled, and the AFIO->MAPR register is set appropri...

Hardware bug in STM32F051K8

Posted on October 05, 2012 at 11:28Hello, Did some more tests on my TIM + DMA issue with also atollic to verify it was not the compiler. I am now pretty sure it is a hardware bug in the STM32F051. I tried almost every configuration possible, but if ...

root by Associate II
  • 1638 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.