2011-04-11 1:56 AM
Hey, Im trying to set up an SPI-bus between the STM32VLDISCOVERY and an external flash memory. I want the STM32-processor to be master and the flash-memory to be slave.
What ive tried to far is simply to set up the GPIOs and also trying to send simple data but i get nothing. Im using an oscilloscope to read Pin7 on PortA on the STM32board. Obviously im doing something wrong but i dont really know what. Probably its some code missing? This is what i have so far: &sharpinclude ''stddef.h'' &sharpinclude ''stm32f10x.h'' &sharpinclude ''stm32f10x_gpio.h'' &sharpinclude <stm32f10x_spi.h> &sharpinclude ''string.h'' &sharpdefine SPI_COMMS SPI1 &sharpdefine PORT_SPI_COMMS GPIOA &sharpdefine PIN_SPI_COMMS_NCS GPIO_Pin_4 &sharpdefine PIN_SPI_COMMS_SCK GPIO_Pin_5 &sharpdefine PIN_SPI_COMMS_MISO GPIO_Pin_6 &sharpdefine PIN_SPI_COMMS_MOSI GPIO_Pin_7 void GPIO_Configuration(void); void SPI_Configuration(void); void RCC_Configuration(void); int main(void) { GPIO_Configuration(); SPI_Configuration(); RCC_Configuration(); for(;;){ SPI_I2S_SendData(SPI1,0xAAAA); } } void SPI_Configuration(void) { SPI_InitTypeDef SPI_InitStructure; /* SPI_MASTER configuration -------------------------------------------------*/ SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Hard; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_4; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI_COMMS, &SPI_InitStructure); /* Enable SPI_MASTER TXE interrupt */ SPI_I2S_ITConfig(SPI_COMMS, SPI_I2S_IT_TXE, ENABLE); /* Enable SPI_MASTER */ SPI_Cmd(SPI_COMMS, ENABLE); } void GPIO_Configuration(void) { GPIO_InitTypeDef GPIO_InitStructure; // Enable SPI1 Pins Software Remapping // //GPIO_PinRemapConfig(GPIO_Remap_SPI1, ENABLE); // Configure SPI_MASTER pins: SCK, MISO and MOSI // GPIO_InitStructure.GPIO_Pin = PIN_SPI_COMMS_SCK | PIN_SPI_COMMS_MISO | PIN_SPI_COMMS_MOSI; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(PORT_SPI_COMMS, &GPIO_InitStructure); GPIO_Init(PORT_SPI_COMMS, &GPIO_InitStructure); } void RCC_Configuration(void) { // Enable GPIO clock // RCC_APB2PeriphClockCmd(PORT_SPI_COMMS, ENABLE); } What am i missing? Thanks in advance for your help!! //Fredrik #spi2011-04-11 9:06 AM
The GPIO pin control registers won't latch new values until it has an active clock.
You don't enable the clocks until after you try to write the GPIO registers. Move the RCC setup so that it is done first. This is such a common oversight that the run-time environment that I wrote does this as the first step, with a weak binding so an application can override the settings if it's especially power-sensitive. I don't expect this to ever to be overridden, since such an application would just explicitly turn off everything it could after configuration. /* The default settings enable all of the the timers and GPIO ports. */ unsigned int __attribute__((weak)) #if 0 _RCC_APB1ENR = APB1ENR_TIM3EN, _RCC_APB2ENR = APB2ENR_IOPDEN | APB2ENR_IOPCEN | APB2ENR_IOPBEN | APB2ENR_IOPAEN | APB2ENR_AFIOEN; #else _RCC_APB1ENR = 0x7fffffff, _RCC_APB2ENR = 0x003fffff; #endif /* This routine is the entry point after reset. * We configure a few essential registers, then leap into main(); */ void __attribute__((naked, used, noreturn)) _crt0(void) { /* Enable peripheral clocks. This bumps the power use up slightly, * but developers benefit from having peripherals work by default * rather than mysteriously not respond. * If the program is power sensitive it can override the weak bindings. */ APB1ENR =_RCC_APB1ENR; APB2ENR = _RCC_APB2ENR;2011-04-12 5:01 AM
Hello and thanks for your help!
I did change the order and now the RCC config is done before the GPIO. But it didn't work for me. I still dont see any signs of datatransfer. Do i need the rest of your code? And where do i put that exactly? Again, thanks for your time and help! //Fredrik2011-04-14 5:11 AM
I got it working. Thanks for your help
2012-10-10 11:35 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.