2012-10-07 8:20 PM
I can get PWM output to work with my F4 MCUs, but I can't get it to work with the F0. My code is below, any ideas? As you can see, I'm not using the STM libraries, I am only using their stm32f0xx.h header for register definitions.
#include ''stm32f0xx.h'' #include ''core_cm0.h'' void TIM1_BRK_UP_TRG_COM_IRQHandler(); // ISR prototype int main() { RCC->AHBENR |= RCC_AHBENR_GPIOAEN; // Enable GPIOA clock GPIOA->MODER |= GPIO_MODER_MODER8_1; // Pin A8 mode = Alt Function GPIOA->AFR[1] |= 0b0010; // Pin A8 alt function = AF2 (TIM1) GPIOA->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR8; // Pin A8 speed = 50MHzRCC->APB2ENR |= RCC_APB2ENR_TIM1EN; // Enable clock
TIM1->PSC = 23; // Prescaler = 23 (1 tick per half microsecond) TIM1->ARR = 19999; // Auto-reload = PWM frequency in half microseconds = 10ms period TIM1->CCMR1 |= TIM_CCMR1_OC1M_1 | TIM_CCMR1_OC1M_2; // OC1M = 110 for PWM Mode 1 output on ch1 TIM1->CCMR1 |= TIM_CCMR1_OC1PE; // Output 1 preload enable TIM1->CR1 |= TIM_CR1_ARPE; // Auto-reload preload enable TIM1->CCER |= TIM_CCER_CC1E; // Enable output for ch1 TIM1->CCR1 = 1800; // CCR1 = Duty cycle in half microseconds = high for 900us TIM1->EGR |= TIM_EGR_UG; // Force update TIM1->SR &= ~TIM_SR_UIF; // Clear the update flag TIM1->DIER |= TIM_DIER_UIE; // Enable interrupt on update event NVIC_EnableIRQ(TIM1_BRK_UP_TRG_COM_IRQn); // Enable IRQ TIM1->CR1 |= TIM_CR1_CEN; // Enable counterwhile(1) {
} } void TIM1_BRK_UP_TRG_COM_IRQHandler() { if(TIM1->SR & TIM_SR_UIF != 0) { // If update flag is set // do stuff here if needed } TIM1->SR &= ~TIM_SR_UIF; // Interrupt has been handled }2012-10-08 1:55 AM
I can recommend a working example from the StdPeripheralLibrary.
There is a ''TIM_PWM_Output'' called project, that does exactly this for 4 channels at once. It is based on the Periph.DriverLib however. You can strip it down and extract the relevant code if you like.2012-10-10 9:43 PM
After about an hour of printing out register values with GDB and comparing my values with the known-good values used in the STM PWM example, I found my error.
Too simple: when using the advanced timer you must set the MOE main output enable bit. Turns out I wasn't using an advanced timer on my F4's, and made a poor assumption when setting up PWM on my F0 :) -FarrellWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.