SPI-Flash
Posted on August 23, 2010 at 20:09SPI-Flash #spi-spi1-remap-pb3
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on August 23, 2010 at 20:09SPI-Flash #spi-spi1-remap-pb3
Posted on October 15, 2012 at 12:50Dear friends.I'm making a program for STM32F051R8 (STM320518-EVAL). And I was using ST-Link.But, When I was write program that use USART2 (PA14/15), I can not connect to the target by ST-Link.I have tried FlashLoad...
Posted on October 07, 2012 at 18:29 The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on October 14, 2012 at 17:22Thank you for existence of such driver. But this driver is unsigned. Virtual com port is very useful for many applications. It is very hard to use unsigned drivers for clients. As ST makes any other drivers and sig...
Posted on June 06, 2012 at 11:30Hello, Always, when I set on the clock in I2C1 or I2C2, in the status register SR2 is the BUSY bit set. Here the code:int main(void) { I2C1_DBG = (I2C_TypeDef *) I2C1_BASE; // for debugging RCC->APB1ENR |= RCC_APB1ENR...
Posted on October 12, 2012 at 15:51Hello,I'm using the CPAL library.During the ''CPAL_I2C_Init ()'' when the I2C clock is set on, the BUSY bit in the status register SR2 is always set too. Why the BUSY bit is set ?I'm using the I2C1 on a STM32F217VG...
Posted on October 13, 2012 at 20:32I need to measure from outside the sampling frequency of a STM32F4 discovery, I have thought about using a pin as an output, and bring it in an alternating manner to VDD and GROUND each time the DMA takes a sample ...
Posted on October 13, 2012 at 20:22when I build my project,an error ''User\main.c(12): error: &sharp136: struct ''<unnamed>'' has no field ''BSRR'' '' was appeared . k yes,I check the '' STM32F2xx_StdPeriph_Lib_V1.1.0 '' of STM32F2XX , it doesn't...
Posted on October 12, 2012 at 12:53 The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on October 11, 2012 at 20:40Hello, I want to share my story about the use of the microprocessor and the problems arising from it. My system consists of a microprocessor ARM Cortex M3 STM32F103RC6 and various peripherals. I use this system to...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.