STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI1 in DMA2 on STM32F4

Posted on October 29, 2012 at 15:16Hi,I'm trying to switch SPI1 to DMA mode. First I just try to enable on RX channel only, but I tried both RX TX, and many configuration, and I can't figure why it doesn't want to start... #define NBR_BYTES_ 15 uint...

neoirto by Associate II
  • 4430 Views
  • 11 replies
  • 0 kudos

GPIO_PinLockConfig() does not work

Posted on October 29, 2012 at 08:54I have a problem. I set my GPIO port pins on GPIOA. When I wanted to lock them I used GPIO_PinLockConfig function, but when the function passed through. It has done nothing. My pins in LCKR lock register was not lo...

searching for TJpgDec example code

Posted on August 04, 2012 at 15:52hello as the tittle says i'm searching for some example code for http://elm-chan.org/fsw/tjpgd/00index.htmli have fatfs working from chan. i have a display up and running. now i only need to find out how to use the ...

arnold by Associate II
  • 5624 Views
  • 20 replies
  • 0 kudos

STM32F4 CPU Configuration Software

Posted on October 29, 2012 at 14:28hello,everyone, I'm developing a STM32F4 CPU configuration software. It can be used to configure pins and to write configuration ''C'' code for you. Please waiting.........

0690X00000602mVQAQ.jpg

unsigned_int and unsigned_short_int compatibility ?

Posted on October 30, 2012 at 13:32 Hi there, May be this is a silly question, but could someone explain me to how we use unsigned int and unsigned short int types together ? Here is an exemple from a simple working code (gpio.c* of STM32 V...

edgar2 by Associate II
  • 1900 Views
  • 2 replies
  • 0 kudos

Cannot set EXTICR register in STM32F205

Posted on June 21, 2012 at 00:14 Following the example for the STM3240G I set up the KEY pushbutton (PG15) as an external interrupt: RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOG, ENABLE); // enable port RCC_APB2PeriphClockCmd(RCC_APB2Peri...

TimerX chain or master example

Posted on October 30, 2012 at 10:10I want to measure distance between two pulses, pulses come from an another timer. Ist there any example for it? #timer-master-slave

stst9184 by Associate II
  • 1013 Views
  • 3 replies
  • 0 kudos

STM32F4Discovery VCP Problem

Posted on October 29, 2012 at 01:55Hello, I am trying to add VCP on STM32F4Discovery but have some issues which I am not able to figure out. When I add this command USBD_Init(&USB_OTG_dev, USB_OTG_FS_CORE_ID, &USR_desc, &USBD_CDC_cb, &USR_cb); in ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.