2012-10-30 2:10 AM
I want to measure distance between two pulses, pulses come from an another timer. Ist there any example for it?
#timer-master-slave2012-10-30 3:53 AM
This is not yet working:(
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); /* Timer 4 is encoder Timer 2 is speed measurement */ TIM_DeInit(TIM4); TIM_DeInit(TIM2); // Configure the timer TIM_EncoderInterfaceConfig(TIM4, TIM_EncoderMode_TI12, TIM_ICPolarity_Rising, TIM_ICPolarity_Rising); /*NVIC_InitStructure.NVIC_IRQChannel = TIM4_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = TIMx_PRE_EMPTION_PRIORITY; NVIC_InitStructure.NVIC_IRQChannelSubPriority = TIMx_SUB_PRIORITY; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); TIM_ClearFlag(TIM4, TIM_FLAG_Update); TIM_ITConfig(TIM4, TIM_IT_Update, ENABLE);*/ /* Select the Master Slave Mode */ TIM_SelectMasterSlaveMode(TIM4, TIM_MasterSlaveMode_Enable); /* Master Mode selection */ TIM_SelectOutputTrigger(TIM4, TIM_TRGOSource_OC1Ref); /* Slaves Configuration: */ TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_ICInitTypeDef TIM_ICInitStructure; TIM_TimeBaseStructure.TIM_Period = 65535; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); TIM_ICInitStructure.TIM_Channel = TIM_Channel_1; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_BothEdge; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_TRC; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0x0; TIM_ICInit(TIM2, &TIM_ICInitStructure); /* Select the slave Mode: Reset Mode */ TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Reset); TIM_SelectInputTrigger(TIM2, TIM_TS_ITR2); /* Enable the Master/Slave Mode */ TIM_SelectMasterSlaveMode(TIM2, TIM_MasterSlaveMode_Enable); // TIM2, TIM4 counter enable TIM_Cmd(TIM2, ENABLE); TIM_Cmd(TIM4, ENABLE);2012-10-30 4:14 AM
How exactly is it not working?
JW2012-10-30 4:38 AM
Hi Jan,
I want to reset a timer 2 on any edge going out from timer 4. Byt timer 2 incremnets up to max.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.