STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTC internal wake-up doesn't wake-up STM32U5

Hello,I have my STM32U575 set to wake-up from standby-mode by the reset button of the Nucleo-U575ZI-Q. Furthermore I want the MCU to wake-up periodically triggered by the RTC. The sample code below just makes the reset button work but the RTC doesn't...

Resolved! shutting down "spare" Cortex-M4

I've taken over this project that is using the STM32h755 CPU. The software is not currently using the Cortex-M4 processor inside the chip. I'm reworking the software so that it will be able to use it sometime in the future. But, until then, I was hop...

Resolved! STM32F429 ADC problem

I am currently using STM32CubeIDE and want to input an external sine wave. The signal has a voltage of 2.6V and a frequency of 10kHz, and I am using DMA + TIM + ADC. The following is the screenshot of my settings. Currently, I can only capture the pe...

tasabao_2-1729413430489.png tasabao_1-1729413412132.png tasabao_0-1729413380782.png tasabao_3-1729413475914.png
tasabao by Associate III
  • 6178 Views
  • 11 replies
  • 1 kudos

Timer input capture into DMA buffer how get position ?

HI, i use CC2 on TIM1 set as input capture measuring pulse period and store in array   /* USER CODE BEGIN TIM1_Init 1 */ LL_DMA_SetPeriphAddress(DMA1, LL_DMA_CHANNEL_3, (uint32_t)&TIM1->CCR2); LL_DMA_SetMemoryAddress(DMA1, LL_DMA_CHANNEL_3, (uint...

MM..1 by Chief III
  • 1907 Views
  • 3 replies
  • 0 kudos

STM32U5A5QJ Part Selection Clarification

Hi,We are currently in the process of selecting components for our project, and we have identified the STM32U5A5QJ9 (STM32U5A5QJ), foot-print size UFBGA 132 7x7x0.6 P 0.5 mm) microcontroller as a potential candidate. However, upon reviewing the datas...

Resolved! SPI display in standby low power mode

Hello,I have a project which demands the device to work in ultra low power mode. I have opted STM32L4R9AI mcu for this project. The problem is i have a spi based lcd display and i need to display the content constantly without flicker even in low pow...

STM32L432 EXTI strange behaviour

Hi,  I have three buttons - START, STOP and CH_SELECT which are serviced using EXTI interrupts. I have also a rotary encoder (A and B pins). Every button line is serviced on a separate IRQ line. Debouncing of the switch and rotary encoder pins is han...

tompa by Associate III
  • 4338 Views
  • 12 replies
  • 1 kudos

Which TIMs support Quadrature encoder

Hello,I am trying to use the quadrature encoder mode of the TIM in the STM32U585VITx, for positioning purposes of a stepper motor movement.According to DS13086, page 79, the general purpose timers (TIM2, TIM3, TIM4, TIM5, TIM15, TIM16, TIM17) support...

Elham by Associate II
  • 5461 Views
  • 12 replies
  • 2 kudos

STM32F07 Timer max. external clock

HiI want to use a STM32F072 (max. 48MHz) to monitor an external clock.The external clock has a frequency of 38.4MHz.My idea is to use timer TIM3 (32bit) as counter and use the external clock as clock source (external clock mode 1).I read the datashee...

Katagia by Associate II
  • 1541 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.