STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using pre-programmed bootloader on STM32G0B0RE

helloI am developping on a STM32G0B0RE, I've learned after finishing my board and everything that boot pin can be used by default.It is not a problem since I have ST-Link for production but I would like to be able to do firmware update through bootlo...

Tiboww_0-1729088556950.png
Tiboww by Associate III
  • 6949 Views
  • 16 replies
  • 0 kudos

Resolved! STM32 CAN Normal mode

Hi All,I am currently working on the CAN normal mode in a custom board with MCU STM32F098RCT6 and CAN transceiver TJA1042. Very first I tried the loopback mode and it was successful. Then I am now trying to interface two custom boards using the norma...

Resolved! STM32F769 DCMI (Digital Camera interface)

Posted on February 16, 2017 at 07:28      1>> We understand thatSTM32F769 DCMI(Digital Camera interface) is able to process YCbCr 4:2:2 and RGB 565. We could see sample camera program in STM32Cube with video input as RGB 565 format to DCMI module and...

Resolved! PA15 as TIM2_CH1 doesn't work on F103RG with SPI 3 on

Hi all,I'm using a F103 on my current project. I have trouble using the PA15 as TIM2_CH1 which is connect to a LED. I also have a serial flash connected via SPI on PB3 to PB5. As long as I don't activate the corresponding SPI timer in the RCC_APB1ENR...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.