STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI Clock problem

Posted on December 21, 2012 at 08:32Hello ALL, I am using stm32f2xxx. I am programing An accelerometer which is interfaced via SPI. The problem i m facing is the clock is not always continous. My HSEValue is 8Mhz. When i get the clcok properly i co...

Unexplained MCO behavior (?) on STM32F372CBT6

Posted on December 26, 2012 at 21:55I'm running an external 26MHz xtal (10ppm) in HSE mode with the right multipliers/dividers to clock my STM32 core at 71.5MHz. Which works great. In addition, I have PA8 configured in MCO mode to drive said 26MHz c...

dandan9 by Associate II
  • 1276 Views
  • 4 replies
  • 0 kudos

ST-Link JTAG Debugger communication error.

Posted on December 21, 2012 at 05:46Hi,I am getting ''Fatal error:ST-Link USB Communication error'' message while my code still runs on board and this is happening when driver is running for longer time.Thanks in advance.

STM32F207 Low Power mode options

Posted on December 13, 2012 at 14:01I can't fine an example of sleep mode configure. Can someone send me a link?If I want to active the UART and RTC in low power mode. What is the lower mode option I can use? #an3430-low-power-mode-stm32f2

Barbie by Associate II
  • 959 Views
  • 1 replies
  • 0 kudos

STM32F107 Virtual Com example - echo needed

Posted on December 27, 2012 at 09:59Hi! I have a problem with usage of ST-example for Virtual Com port. I have STM32F107 on my board. Example is downloaded correctly and all seems workable. The thing is that my board is not standard evaluation board...

morpeh89 by Associate II
  • 775 Views
  • 0 replies
  • 0 kudos

STM32F107 USB Virtual Com Port - problem

Posted on December 19, 2012 at 14:11Hi! I have a problem using USB as Virtual Com port on STM32F107. I use example code for USB CDC from IAR. I have two boards - with STM32F103 and STM32F107. The first one works properly with my code. When I use the...

morpeh89 by Associate II
  • 1192 Views
  • 1 replies
  • 0 kudos

STM32F207 sample 1 ch ADC

Posted on December 24, 2012 at 12:41Can I sample dedicate 1 channel without the need to put it in the scan list as the first and write Number of ch to scan 1?As I see it it is impossible.Regardsbar. #stm32f207-adc-1-ch-sample

Barbie by Associate II
  • 2267 Views
  • 5 replies
  • 0 kudos

problem about I2S3

Posted on December 20, 2012 at 11:09I get a problem when using I2S3 of STM32F107. when I2S3 works at slave mode, the MCLK can not be created. What I want to ask is why there is no MCLK output, when I2S3 working at slave mode. Or maybe the I2S3 confi...

hw12xian by Associate II
  • 1804 Views
  • 3 replies
  • 0 kudos

stm32 temperature sensor

Posted on December 24, 2012 at 04:29hi,how can I use the STM32 built-in temperature sensor? the STLM20_ReadTemp() function stops the program and I really need to get this to work.thanks #stm32 #stlm20

przemek by Associate II
  • 2377 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.