2012-12-20 11:32 PM
Hello ALL,
I am using stm32f2xxx. I am programing An accelerometer which is interfaced via SPI. The problem i m facing is the clock is not always continous. My HSEValue is 8Mhz. When i get the clcok properly i could see RXNE flag and TXE flag set and it receives valid data. But when i dont get the clock properly i see only TXE flag set. Below is my init, read and write codesvoid GPIO_Configuration(void)
{ GPIO_InitTypeDef GPIO_InitStructure;RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA ,ENABLE);
GPIO_InitStructure.GPIO_Mode=GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed=GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;_InitStructure.GPIO_Pin=SPI1_SCK_PIN;
GPIO_Init(SPI1_GPIO_PORT,&GPIO_InitStructure);GPIO_InitStructure.GPIO_Pin=SPI1_MOSI_PIN;
GPIO_Init(SPI1_GPIO_PORT,&GPIO_InitStructure);GPIO_InitStructure.GPIO_Pin=SPI1_MISO_PIN;
GPIO_Init(SPI1_GPIO_PORT,&GPIO_InitStructure);GPIO_PinAFConfig(GPIOA,SPI1_SCK_SOURCE,GPIO_AF_SPI1);
GPIO_PinAFConfig(GPIOA,SPI1_MOSI_SOURCE,GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA,SPI1_MISO_SOURCE,GPIO_AF_SPI1);/*Configure CS pin in output pushpull mode*/
GPIO_InitStructure.GPIO_Pin = SPI1_CS_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;GPIO_Init(SPI1_GPIO_PORT, &GPIO_InitStructure);
}void SPIConfiguration(void)
{unsigned char ucdummy;
static char ucindex = 20;unsigned char rxbuf[20];
void SPI_Config()
{ SPI_InitTypeDef SPI_InitStructure;RCC_APB2PeriphClockCmd (RCC_APB2Periph_SPI1, ENABLE);
/*SPI initializations*/
SPI_InitStructure.SPI_Direction=SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode=SPI_Mode_Master; SPI_InitStructure.SPI_DataSize=SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL=SPI_CPOL_High; SPI_InitStructure.SPI_CPHA=SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS=SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler=SPI_BaudRatePrescaler_2; SPI_InitStructure.SPI_FirstBit=SPI_FirstBit_MSB; //SPI_InitStructure.SPI_CRCPolynomial=7; SPI_InitStructure.SPI_CRCPolynomial=0;SPI_Init(SPI1,&SPI_InitStructure);
SPI_SSOutputCmd(SPI1,ENABLE); SPI_Cmd(SPI1,ENABLE); }uint8_t SPIXLWriteData(uint8_t Add, uint16_t Data)
{ uint32_t TimeOut;while ((SPI_I2S_GetFlagStatus(SPI1,SPI_I2S_FLAG_BSY)))
{ if (TimeOut--==0) { return SPI_ERROR; } } CS_LOW(); SPI_I2S_SendData(SPI1, ADXL345_W|Add); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); ClrRcvBuf(); SPI_I2S_SendData(SPI1, Data); ClrRcvBuf(); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_BSY) == SET); CS_HIGH();return 1;
}uint8_t SPIReadData(uint8_t RegisterAddress, uint8_t NoOfRgisters)
{ uint32_t TimeOut; uint16_t RxBuffer; /* Select Slave*/ CS_LOW(); /*Make sure the bus is not busy*/ while ((SPI_I2S_GetFlagStatus(SPI1,SPI_I2S_FLAG_BSY))) { if (TimeOut--==0) { return SPI_TIMEOUT_ERROR; } } //RxBuffer = SPI_I2S_ReceiveData(SPI1); SPI_I2S_SendData(SPI1, XL345_R|RegisterAddress);ClrRcvBuf();
RxBuffer=SPI_I2S_ReceiveData(SPI1); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); //dummy byte*/ SPI_I2S_SendData(SPI1, 0x00); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET); the RxBuffer = SPI_I2S_ReceiveData(SPI1); while(SPI_I2S_GetFlagStatus(SPI1,SPI_I2S_FLAG_TXE) != SET); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_BSY) == SET); CS_HIGH();return RxBuffer;
}void SPIXLReadSequence(uint8_t reg,uint8_t count)
{ uint8_t i = 0; CS_LOW(); SPI_I2S_SendData(SPI1, ADXL345_R | ADXL345_MB | reg); ClrRcvBuf(); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); SPI_I2S_SendData(SPI1, 0xFF); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET); data[i]= SPI_I2S_ReceiveData(SPI1); i++; } while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_BSY) == SET); CS_HIGH();}
#spi2012-12-21 4:40 AM
You have to send data for the clocks to be generated. As the transmit data clocks out, the receive data clocks in. Reading the DR just clears a flags, and provides the register content, it does not initiate a transfer. SPI_I2S_ReceiveData() just reads the DR, nothing else.
2012-12-23 8:47 PM
2012-12-27 10:20 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.