STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC in STM32F4 Discovery

Posted on January 02, 2013 at 08:06hi:     i found that ADC12 and ADC123 in STM32F4 Discovery.  How Can I use them?    or whats the way to use ADC on STM32F4Discovery? I have library of STM32F4xx.c in that ADC1, ADC2, ADC3 are only defined? which ar...

its by Associate II
  • 1436 Views
  • 1 replies
  • 0 kudos

Problem on using USART with DMA

Posted on January 01, 2013 at 20:52Hello, I am implementing a UART driver using circular queue scheme, and found a minor problem with it. When I put a new character after DMA channel 5 finishes its transfer - i.e. put a new character when DMA_CNDTR5...

how to use Index Track in quadrature encoder mode

Posted on December 26, 2012 at 18:15have 2 timer channels (CH1+CH2) setup in quadrature encoder mode and all things work fine. The encoder (Avago HEDS 5540) has a third index channel with very narrow pulse per revolution. Is ist possible to use this...

jveith by Associate II
  • 3041 Views
  • 3 replies
  • 0 kudos

FAT in SD Card

Posted on December 26, 2012 at 06:36HiThis question is meant specifically for Clive1. Your earlier post on FAT at https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a%2f%2fmy.st.com%2fpublic%2fSTe2ecommun...

nakulrao by Associate II
  • 4581 Views
  • 10 replies
  • 0 kudos

Loading user compiled modules

Posted on December 29, 2012 at 20:09I am looking for a way to have a simple system that runs a multi-thread main program on the processors memory and then has the ability to read a SD card and load user compiled modules into different threads and ru...

Read potentiometer Value ?

Posted on December 29, 2012 at 15:19 Hi, I want to program a potentiometer connected in PC2 as input using STM32F4 I use this program GPIO_InitTypeDef GPIO_InitStructure; ADC_InitTypeDef ADC_InitStructure; /*...

bmwael1 by Associate II
  • 3108 Views
  • 6 replies
  • 0 kudos

What could stop SWD from working?

Posted on December 28, 2012 at 21:18Im running an application on a STM32F103R8T6. The debug interface works as expected most of the time. But occasionally I can't connect neither with an ST-Link nor IAR I-jet. The code runs normally while trying to ...

USB DFU fails on STM32F205

Posted on December 21, 2012 at 21:46I'm attempting to get DFU over USB working on a STM32F205VET6. Chip marking: STM32F205 VET6        X HPABG    VG KOR   HP   225 Computer Windows 7 64-bit Intel Pentium dual core processor The BOOT0 input is derive...

external RAM STM32F4

Posted on December 27, 2012 at 05:38 hi I have memory constraints to hold image data greater than 32768 bytes. Can I use external RAM/memory for that to overcome this limitation so that I can get high resolution image data? will that fast enoug...

its by Associate II
  • 3011 Views
  • 6 replies
  • 0 kudos

how to find the MAC adress of F407 ?

Posted on December 27, 2012 at 14:25hello forum, I am trying to send and receive UDP packets from my F407 to PC however as shown below I need to know MAC adress of my F407struct eth_header { //ether frame uint8_t ether_src[6]; ...............memcpy(...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.