2012-04-06 9:41 AM
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
/* TIM config */ GPIO_InitTypeDef GPIO_InitStructure; /* TIM4 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE); /* LEDs are on GPIOD */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ; GPIO_Init(GPIOD, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOD, GPIO_PinSource12, GPIO_AF_TIM4); GPIO_PinAFConfig(GPIOD, GPIO_PinSource13, GPIO_AF_TIM4); GPIO_PinAFConfig(GPIOD, GPIO_PinSource14, GPIO_AF_TIM4); GPIO_PinAFConfig(GPIOD, GPIO_PinSource15, GPIO_AF_TIM4); /* pwm set up */ /* Compute the prescaler value */ PrescalerValue = (uint16_t) ((SystemCoreClock /2) / 21000000) - 1; /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = 665; TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure); /* PWM1 Mode configuration: Channel1 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 0; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM4, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM4, TIM_OCPreload_Enable); /* PWM1 Mode configuration: Channel2 */ TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 0; TIM_OC2Init(TIM4, &TIM_OCInitStructure); TIM_OC2PreloadConfig(TIM4, TIM_OCPreload_Enable); /* PWM1 Mode configuration: Channel3 */ TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 0; TIM_OC3Init(TIM4, &TIM_OCInitStructure); TIM_OC3PreloadConfig(TIM4, TIM_OCPreload_Enable); /* PWM1 Mode configuration: Channel4 */ TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 0; TIM_OC4Init(TIM4, &TIM_OCInitStructure); TIM_OC4PreloadConfig(TIM4, TIM_OCPreload_Enable); TIM_ARRPreloadConfig(TIM4, ENABLE); /* TIM4 enable counter */ TIM_Cmd(TIM4, ENABLE); /* DEMO */ int brightness = 0; while(1) // Do not exit { brightness++; TIM4->CCR3 = 333 - (brightness + 0) % 333; // set brightness TIM4->CCR4 = 333 - (brightness + 166/2) % 333; // set brightness TIM4->CCR1 = 333 - (brightness + 333/2) % 333; // set brightness TIM4->CCR2 = 333 - (brightness + 499/2) % 333; // set brightness for(i=0;i<10000;i++); // delay for(i=0;i<10000;i++); // delay for(i=0;i<10000;i++); // delay }} #stm32f4-pwm-led2012-04-19 10:36 AM
2012-12-20 2:33 AM
What is this operator '%' (brightness + 0) % 333 ?
if
brightness
= 1 =>(brightness + 0) % 333 = 1
if
brightness
= 332 =>(brightness + 0) % 333 = 332
if
brightness
= 333 =>(brightness + 0) % 333 = 0
if
brightness
= 334 =>(brightness + 0) % 333 = 1
if
brightness
= 665 =>(brightness + 0) % 333 = 332
if
brightness
= 666 =>(brightness + 0) % 333 =
0
if
brightness
= 667 =>(brightness + 0) % 333 =
1
2012-12-20 4:34 AM
What is this operator '%'
That would be the C language's modulus (remainder) operator.2012-12-26 6:40 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.