STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 ADC3 setup fails

Hi,I am trying to set-up the ADC3 for STM32H7 but the HAL_ADC_Init() fails ? After debugging, I see that the function LL_ADC_IsInternalRegulatorEnabled() fails in HAL_ADC_Init(). I also see that DEEPPWD is 0 on reset but the datasheet say that it sho...

Daan1_0-1729897920043.png
Daan1 by Associate II
  • 3952 Views
  • 7 replies
  • 0 kudos

Resolved! CAN Communication in Loopback mode with STM32F407

I want to implement CAN Communication in Loopback mode in which I have added Can interrupt mode . In Tx interrupt it will sent data after every 1000 m/s and data increment . In Rx interrupt it will read the sent data. I compiled the code and it will ...

Resolved! STM32H7 stuck on read protect

Hi, I am using STMH755ZI chip and i have a custom board created using this. I have code which receives a character through UART and jumps to DFU mode for flashing. I am not using ST LINK and in case of emergency, i kept BOOT0 pin open so that i can g...

kps98_0-1729412353225.png kps98_1-1729412376730.png
kps98 by Associate III
  • 3379 Views
  • 5 replies
  • 0 kudos

SPL support for STEVAL-ESC001V1 or X-NUCLEO-IHM08M1?

Hello.Is there an example F/W for STEVAL-ESC001V1 or X-NUCLEO-IHM08M1 that is SPL compatible?I need to continue to use the Standard Peripheral Library (SPL) to utilize the existing code.If there is a way to create or convert the project by X-CUBE-MCS...

Writing Option Bytes on STM32F1

Hello,Im developing an program that controls an ST-Link to flash an STM32F1. The program needs to be able to remove RDP on the MCU its trying to flash.Im doing the following steps:1) Unlocking Flash - confirmed working (registers confirm)2) Unlocking...

guandast_2-1729788721514.png guandast_1-1729788647355.png
guandast by Associate II
  • 2502 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G474 Unable to initialize more than one ADC

Hi All,I'm trying to setup 2 ADCs in continous mode but I'm failing miserably. In CubeMX I set the first ADC in continuous mode, triggered by software, then HAL_ADC_Start_IT(&hadc1); and it works as expected (I have a callback to read the value).Then...

aldoir by Associate
  • 1847 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.