cancel
Showing results for 
Search instead for 
Did you mean: 

SPL support for STEVAL-ESC001V1 or X-NUCLEO-IHM08M1?

Choibogue
Associate II

Hello.

Is there an example F/W for STEVAL-ESC001V1 or X-NUCLEO-IHM08M1 that is SPL compatible?
I need to continue to use the Standard Peripheral Library (SPL) to utilize the existing code.
If there is a way to create or convert the project by X-CUBE-MCSDK to SPL compatible, that would be the best.

Thank you!

0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.