STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Debuging code create by IAP

Posted on April 03, 2013 at 08:34When I write a code with the BootLoader as IAP there is a question how i can debug it. I wander why it nit arise before. I put the BootLoader code on the debuger and run with it all the way till it finish to write t...

Barbie by Associate II
  • 1090 Views
  • 1 replies
  • 0 kudos

IWDT refresh and reset

Posted on March 27, 2013 at 06:42Hello All, I am using stm32f2 series. I have initilized Independent watch dog timer. My intention is , when there is some probelm in the peripherals, i need to reset the device (microcontroller) after few seconds. So...

Stm32 Embedded GUI Lib V2.0.0

Posted on October 27, 2011 at 08:20Hi Whilst compiling the demo with warnings enabled I get the following error ''src/graphicObject.c:1476:7: warning: the address of 'pPage' will always evaluate as 'true''' This error is associated with the followi...

divner by Associate II
  • 6075 Views
  • 13 replies
  • 0 kudos

Hardware trigger

Posted on March 31, 2013 at 20:24 Hello, i have CLK which is generated by ADC, and i need to generate SI signal as shown in this picture. I used software version, but it is very unstable, and if i recompile that, it can completely mess up t...

0690X000006054lQAA.png
linas2 by Associate II
  • 4674 Views
  • 11 replies
  • 0 kudos

FSMC Memory Issue

Posted on April 02, 2013 at 08:24 Hi , I am testing out the following file ,GLCD_16bitIF_STM32F2xx.c from KEIL #define LCD_BASE (0x60000000UL | 0x00000000UL) #define LCD_REG16 (*((volatile unsigned short *)( LCD_BASE ))) #define LCD_DA...

Is there a ST-LINK_CLI.exe for ST-Link /V2?

Posted on August 09, 2011 at 08:16Hi All, I want to use ST-Link/V2 for downloading to flash in KEIL IDE. At present when you use the flash loader to download. It does not do anything no error nothing. just does not download it just says Load ''D:\\K...

jai2 by Associate
  • 1395 Views
  • 2 replies
  • 0 kudos

Maximum ADC clock frequency?

Posted on March 28, 2013 at 12:18Hi! I have a question regarding the maximum clock frequency for the ADC. The data sheet on STM32F407 gives maximum clock frequency for ADC as 36 MHz (Doc ID 022152, Rev 3, page 124) for power supply of 3.6 V. Howev...

dusan2 by Associate III
  • 5642 Views
  • 4 replies
  • 0 kudos

problem map a struct to Backup registers

Posted on April 01, 2013 at 11:06 I got a problem map a struct to Backup registers what I do is: /******************************************************************************************/ typedef struct {     uint16_t actPageNo;     uint16_t sollQ...

jgnoss by Associate III
  • 2748 Views
  • 7 replies
  • 0 kudos

MCBSTM32F200 exemples

Posted on March 28, 2013 at 15:14Hi all,I am trying to compile the exemples that keil provide with MCBSTM32F200 in the folder C:\Keil\ARM\Boards\Keil\MCBSTM32F200 but I got problems in some exemples that are almost the same:In FTP demo i got  ''all ...

felipe by Associate II
  • 1541 Views
  • 2 replies
  • 0 kudos

STM32 RTC alarm and counting problem

Posted on April 01, 2013 at 08:21 Hi, I want to use the RTC's alarm A for waking up from standby. However, I cannot get the alarm interrupt. I am initialising timer 3 for interrupting every 5 seconds and reading the rtc within the interrupt hand...

adithya2 by Associate II
  • 2039 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.