2011-08-08 11:16 PM
Hi All,
I want to use ST-Link/V2 for downloading to flash in KEIL IDE. At present when you use the flash loader to download. It does not do anything no error nothing. just does not download it just says Load ''D:\\Keil_MDK\\ARM\\INC\\ST\\3.5\\STM32F10x_StdPeriph_Lib_V3.5.0\\Project\\STM32F10x_StdPeriph_Template\\MDK-ARM2\\STM32100E-EVAL\\STM32100E-EVAL.AXF'' Is there a ST-Link_CLI.exe for ST-Link/V2. In keil I want to do external flash programming. Thanks and Regards, Jai2013-03-01 11:02 AM
2013-04-02 3:04 AM
Hello Felipe,
''Same problem for me...'', how exactly? Issue with the FlashLoader? Please note that allowed file formats are .bin, .hex or .s19 and not .axf. If you are looking for the ST-LINK_CLI.exe, it is available with the ST-Link Utility package downloadable fromhttp://www.st.com/web/en/catalog/tools/PF258168
. Best Regards, ST.MCUTo give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.