STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4Discovery interrupt on PortD Pin0

Posted on March 30, 2013 at 15:09Hello, i used a STM32F4Discovery. My code is at the end of this text. The programm should release a interrupt by rising edge on PortD Pin0. Then the LED toggle on PortD Pin14. This does not work. Where is the mistak...

Watchdog timer problem

Posted on March 22, 2013 at 11:27Hi, I am using the STM32L151VB in a custom board. The problem I have is with the watchdog timer. The maximum time out is too less for me to do anything that I intend to. Right now I am using the TIM4 timer for a long...

adithya2 by Associate II
  • 3251 Views
  • 5 replies
  • 0 kudos

USART_Printf demo with STM32L152-EVAL

Posted on March 29, 2013 at 06:45Dear everyone,     USART_Printf demo provided in STM32L1xx_StdPeriph_Lib_V1.2.0 can't run on STM32L152-EVAL. I found that there is no output at ST3241EB Pin 11. However, I use PC10/PC11 (UART3) with another MAX232, t...

xinjin by Associate II
  • 1536 Views
  • 2 replies
  • 0 kudos

Using NRST for system reset through hardware

Posted on March 30, 2013 at 19:25HiI would like to apply an automatic system reset in case a particular condition in my system is met. I already know how to apply a system reset through software. Now I want also to do it via hardware. If If I pull p...

terence-b by Associate II
  • 1993 Views
  • 3 replies
  • 0 kudos

USART and stop bits

Posted on June 23, 2011 at 23:58In playing around with USART3, I'm attempting to configure it for DMX (250000 baud, 8 data bits, 2 stop bits).  In fact, when configured this way, what actually seems to happen is that any data I attempt to send is ac...

slandrum by Associate II
  • 6560 Views
  • 9 replies
  • 0 kudos

NHD-C12832A1Z with the STM32F103

Posted on March 30, 2013 at 18:41I need some help. I have a board with a STM32F103CB micro and an NHD-C12832A1Z 128x32 pixel graphic LCD display with built in ST7565R controller. My problem is that I can not get the display to display anything. The ...

STM32F407 nested interrupts

Posted on March 31, 2013 at 13:18Once again I feel really stupid. I can't get nested interrupts working.In the attached file there are three functions, NVIC_Configuration(), SysTick_Handler() and TIM6_DAC_IRQHandler().I intend the SysTick interrupt ...

STM32F4: Using two DMA streams with single request

Posted on March 21, 2013 at 08:25Device: STM32F405. Is it possible to use two DMA streams with single request? For example, connect DMA2_Stream0 to channel 6 (TIM1_TRIG) and DMA2_Stream4 to channel 6 (TIM1_TRIG, too). I want to start two diffirent D...

Jumping to a memory location..bootloader C code

Posted on March 30, 2013 at 22:15Hi, In our system, I have to be able to update the application code. Therefore I believe I need to copy the application to memory location 0x8000000 and then jump to this location...basically a small bootloader of so...

stenasc by Senior
  • 1032 Views
  • 1 replies
  • 0 kudos

Beginner there is any pdf reference about stm32

Posted on March 30, 2013 at 09:21I have experienced with AVR MCU-8bits programs. When I was begin to AVR MCU, there is an official reference that prepared by Atmel itself for developer to understand what register should be initialed in order to have...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.