STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Meaning of ''FM+ capable''

Posted on June 19, 2013 at 16:25Hello to everyone!What does it mean the ''FM+ capable'' feature of a pin? There is 5V tolerant, and 5 V tolerant I/O, FM+, pin (STM32F051x4 datasheet - pin PB6, PB7, PB8, PB9) and what is the diference? This feature i...

Typos in Reference Manuals for STM32F3

Posted on June 05, 2013 at 22:36  told me to report on this forum any corrections needed in reference docs and code. These corrections apply to the latest published reference manuals for STM32F3xx: RM0316: STM32F302xx, STM32F303xx and STM32F313xx...

gfuehrer by Associate II
  • 2373 Views
  • 5 replies
  • 0 kudos

stm32f1xx.h to stm32f4xx.h

Posted on June 17, 2013 at 14:52I need to update this function to stm32f4xx.h.void delay_us(u32 Nus){     SysTick_SetReload(delay_fac_us * Nus);    SysTick_CounterCmd(SysTick_Counter_Clear); // error: 'SysTick_Counter_Clear' undeclared (first use in...

ricardo by Associate II
  • 3815 Views
  • 7 replies
  • 0 kudos

Refreshing DMA source address

Posted on June 17, 2013 at 08:50 Hello, I want to put the data from buffer(RAM) to the GPIO port(transmit) and from another GPIO port to the buffer(RAM)(receive) with the 2MHz clock. So I'm using DMA with input capture mode of the timer. ...

TIM2 Interrupt problem

Posted on June 18, 2013 at 11:25I write this code witch turn on the 4 leds of the stm32 when pushing the bouttan and after it wait for some time and turn off the 4 leds. I checked the code without the delay it work fine but whith the delay the progr...

STM32F405RG USB FS unexpected Interrupt

Posted on June 17, 2013 at 18:30I build my own STM32F405RG Stamp and try now to get the USB FS running. For to make good progress I use the libraries, which are available for the stm32F407 Discovery. I use Atollic True Studio Lite and ST-Link/V2 SWD...

mgmv05 by Associate II
  • 1129 Views
  • 1 replies
  • 0 kudos

STM32 Accelometer

Posted on June 17, 2013 at 17:07hello people i'm using IAR  IDE and i'm trying to make a program which get accelo values (x and y) and put them on lcd  this is my code and it didnt work i dont know why: ****************************** #include ''stm...

On board ST-LINK and Windows 8

Posted on November 29, 2012 at 13:34Hello,I have same problem with my ST Discovery board on Windows 8. After I connect board to PC, windows was trying to install driver - but unsuccessful because driver files does´t contain a digital signature. In ...

hospodar by Associate III
  • 1502 Views
  • 3 replies
  • 0 kudos

systick always 3 times what it should be

Posted on June 18, 2013 at 05:03I've tested the example systick app and it worked, but my (keil) app will not work. I'm just trying to blink a light on a 2 sec interval, super frustrating.the project settings have the system clock at 25mhz. I'm usin...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.