2013-06-19 7:25 AM
Hello to everyone!
What does it mean the ''FM+ capable'' feature of a pin? There is 5V tolerant, and 5 V tolerant I/O, FM+, pin (STM32F051x4 datasheet - pin PB6, PB7, PB8, PB9) and what is the diference? This feature isn't mentioned anywhere.Thank You. #high-current #aggresive2013-06-19 7:54 AM
The I/O speed configuration is bypassed in FM+ I/O mode. Refer to the STM32F05xxx reference manual RM0091 for a
description of FM+ I/O mode configuration. .. The high sink LED driver capability (only available on the PB9 pin) can be activated through the I2C_PB9_FM+ bit in the SYS_CTRL register and used to sink the high current needed to directly control an infrared LED. .. 20 mA output drive for FM+ mode .. Bits 19:16 I2C_PBx_FM+: Fast Mode Plus (FM+) driving capability activation bits. These bits are set and cleared by software. Each bit enables I2C FM+ mode for PB6, PB7, PB8, and PB9 I/Os. 0: PBx pin operates in standard mode. 1: I2C FM+ mode enabled on PBx pin, and the Speed control is bypassed.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.