2013-06-17 8:03 PM
I've tested the example systick app and it worked, but my (keil) app will not work. I'm just trying to blink a light on a 2 sec interval, super frustrating.
the project settings have the system clock at 25mhz. I'm using stm32f4 eval board.// in that system.c file#if !defined (HSE_VALUE) #define HSE_VALUE ((uint32_t)25000000) /*!< Value of the External oscillator in Hz */#endif /* HSE_VALUE *//** * @brief In the following line adjust the External High Speed oscillator (HSE) Startup Timeout value */#if !defined (HSE_STARTUP_TIMEOUT) #define HSE_STARTUP_TIMEOUT ((uint16_t)0x0500) /*!< Time out for HSE start up */#endif /* HSE_STARTUP_TIMEOUT */ #if !defined (HSI_VALUE) #define HSI_VALUE ((uint32_t)16000000) /*!< Value of the Internal oscillator in Hz*/#endif /* HSI_VALUE */ // in startup case 0x01: if (SysTick_Config(SystemCoreClock / 1000)) { /* Capture error */ while (1); } nodeTimeID = data[j++]; break;// elsewhere while(1) { GPIOD->BSRRL = GPIO_Pin_14; // hi Delay(2000); GPIOD->BSRRH = GPIO_Pin_14; // lo Delay(2000); }2013-06-17 8:21 PM
Check if you have HSE_VALUE defined as part of the project meta-data.
Make sure the settings for HSE_VALUE are coherent with the board, and the the PLL settings in the system_stm32f4xx.c are too. The STM32F4-Discovery has an 8 MHz crystal. Confirm clocks via MCOx pins. Try configuring with HSIWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.