STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F3 Discovery File Compatibility

Posted on June 17, 2013 at 17:43I'm currently working with a STM32F3-Discovery board which has the STM32F303VC microcontroller on it.  I'm planning on eventually using the STM32F373C8 on my board, but I want to test out some code and get comfortable...

mattfox by Associate II
  • 1028 Views
  • 2 replies
  • 0 kudos

Setting SPI1 freq for SD card = 24Mhz

Posted on June 17, 2013 at 12:32I am using STM32F205 with 120Mhz interanl PLL(HSI).I have to interface SD Card on SPI with <= 24Mhz. Problem is with 120Mhz sysclk I can only obtain SPI-30Mhz(can't use of SD), 15Mhz(too slow)and other lower freq.Now ...

Blinking LED based on IWDG counter

Posted on June 15, 2013 at 13:38Hi, In our system, our main code loop repeats every 12 seconds and refreshs the watchdog counter. When refreshing the counter, I toggle an LED. The only problem is the blink period. I would lke the watchdog running LE...

stenasc by Senior
  • 2963 Views
  • 9 replies
  • 0 kudos

Datasheet correct for LQFP64 F37x or not?

Posted on June 15, 2013 at 03:44I'm looking for confirmation (first hand knowledge, please -- speculation is usless) that PA3 on the F37x and F38x are in fact at pin 18 and not on pin 17 as it is for all the other LQDP64-packaged F1xx, F2xx, F3xx, a...

gfuehrer by Associate II
  • 1384 Views
  • 2 replies
  • 0 kudos

Self-test library for STM32F2xx?

Posted on October 05, 2012 at 09:45Hello, for STM32F1xx a self-test library is available as described in AN3307. Is a similar library available for STM32F2xx? Or can the same library be adapted for STM32F2xx? Bodo

extern by Associate
  • 1580 Views
  • 2 replies
  • 0 kudos

CLKOUT feature on STM32F205

Posted on June 17, 2013 at 11:01I have used following code to get CLKout on PC9 but it didn't work:Sysyteminit() was called earlier.     /*Enable or disable the AHB1 peripheral clock */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); /*Configu...

Stm32 programing problem

Posted on June 16, 2013 at 12:38I'm using IAR. My board wold not get programated. In fact the program annonce that the program was successfully downloaded and the debug mode is opned but the program in the stm32 wold not change :\ when I chek the de...

Internal Sram Read And Write

Posted on June 16, 2013 at 06:32Hey guys,I would be very grateful if someone help me for the following issue.I want to compile and save some information in an indoor internal SRAMmicrocontroller when power supply of microcontroller goes offline,thos...

htc by Associate
  • 1041 Views
  • 1 replies
  • 0 kudos

STM32F2xx Bootloader Sectors allocation

Posted on June 15, 2013 at 08:00HI, I'm starting to implement my own bootloader for STM32F2xx. Currently I plan to support UART, USB and ETH. Also I plan to use EEPROM emulation. Implementation of USB and ETH (TCPIP Socket) takes about 30K. So To b...

dimax by Senior
  • 2735 Views
  • 9 replies
  • 0 kudos

Where is the NVIC_InitStructure?

Posted on June 15, 2013 at 22:18I am trying to configure the NVIC for the first time. In looking online for help, most project reference these functions:   NVIC_InitTypeDef NVIC_InitStructure;   /* Enable the TIM2 gloabal Interrupt */   NVIC_InitStr...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.