STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4Discovery counter problem,

Posted on July 28, 2013 at 22:22I have problem with timer - I want use one as simply counter of external impulses. Now I have (with too many unnecessary settings), but counter not work. I want use eg. TIM1, then I should use GPIO setting as AF for T...

alprof by Associate II
  • 1200 Views
  • 2 replies
  • 0 kudos

Strange PD2 behavior on STM32F405RG

Posted on July 25, 2013 at 10:40 Hi ! I'm trying to use PD2 on my STM32F405RG as GPIO output. I think i configured it correctly but it does not switch. Here is my code, it is not that difficult.... GPIO_InitTypeDef GPIO_InitSt...

Eich by Associate III
  • 2349 Views
  • 6 replies
  • 0 kudos

STM32F4 Discovery ADC+USART

Posted on July 28, 2013 at 19:03Hallo Guys,I'm working on project which implies analog to digital conversion and at same time transfering the converted data to the PC through the serial port. I've read couple of examples and was led to the following...

mahmoud by Associate
  • 1743 Views
  • 2 replies
  • 0 kudos

UART interrupts STM32

Posted on July 29, 2013 at 01:31I'm using UART for comunication with PC and I want to implement some interrupts. It seems to me that USART_IT_TXE  and  USART_IT_TC  are the same. Can someone explane me what is the difference between them? #stm32-...

marko by Associate II
  • 1241 Views
  • 1 replies
  • 0 kudos

Basic SDIO on F4 discovery board

Posted on September 15, 2012 at 09:58Can anyone please provide me with a link to some basic, low level, 4-bit SDIO interface code compatible with the STM32F4VGT? I'm not looking for it to support a file system(yet), I just want to be able to read by...

STM32F3 Discovery Quadrature Encoding

Posted on June 21, 2013 at 22:44I'm working on getting quadrature encoding working through either TIM1 or TIM8.  I searched the past topics on this forum, but I can't tell how mine is different/ why it isn't working.  I'm using USART to debug the co...

mattfox by Associate II
  • 6082 Views
  • 15 replies
  • 0 kudos

Multiple math functions calling issue

Posted on July 27, 2013 at 15:46Hi, I've noticed weird problem when calling few math functions few times in a row or a loop like: c = sin(3.0)+sin(5.0)+sin(5.0)+sin(5.0)+sin(5.0)+sin(5.0)+sin(4.0); Actually I don't know what's going wrong but my app...

problem

Posted on July 27, 2013 at 10:02when i connect 16GB flash disk    ,  stop in  USB_Host.EnumState = ENUM_GET_FULL_DEV_DESCUSB_Host.gState=HOST_CTRL_XFERUSB_Host.gStateBkp =HOST_ENUMERATIONUSB_Host,RequestState=CMD_WAITbut when connect 4Gb usb flash d...

LSM303dhlc stm32

Posted on July 26, 2013 at 22:06Hi! please help to solve the problem. I use a compass and a compile-time compiler gives me the following:Error[Li005]: no definition for ''SYSCFG_EXTILineConfig'' [referenced from C:\Users\Ëåâàí\ Error[Li005]: no defi...

svarog995 by Associate II
  • 1443 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.