STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

where can i download the STemWin Library

Posted on July 25, 2013 at 08:44i wanna used the STemWin Library to display the picture and video,i download the AN4323 Application note,it introduce  how to use theSTemWin Library ,however ,i google it, but find nothing.i used the STM32F439 to cont...

aizhixi by Associate II
  • 1488 Views
  • 2 replies
  • 0 kudos

Attn Clive.. and a few questions

Posted on July 26, 2013 at 22:15Sorry had to do this, but this is a request for Clive. There is no PM capability on these forums. If possible, Clive, could you please drop me a mail at admin AT 43oh.com I'd be grateful if you do. This does not rela...

STM32F373 USB DFU Bootloader

Posted on July 25, 2013 at 23:25I'm working with a new device, and I'm trying to load to flash memory via the bootloader in DFU mode.  I'm pretty new to this whole idea, so I'm somewhat confused as to how this works.  From the documents I can find p...

mattfox by Associate II
  • 1862 Views
  • 5 replies
  • 0 kudos

First boot on new target board

Posted on June 19, 2013 at 18:30Powered up newly designed board today. Of course it seems not to work. :( Its based on Discovery board. I currently have only the STM portion populated. The Oscillator pins are both low. Using a 8 Mhz Xtal and 20 pf c...

VE7HR by Associate II
  • 2008 Views
  • 5 replies
  • 0 kudos

problem with leaving from standby mode

Posted on July 26, 2013 at 12:06 Hi, i've got a problem with leaving from standby mode, both by RTC Alarm and WKUP pin. This is my code:int main( void ) { #ifdef DEBUG debug(); #endif prvSetupHardware(); GPIOC->ODR |= (u16)0x0040; PWR_EnterSTANDBY...

kkkuba by Associate II
  • 1388 Views
  • 2 replies
  • 0 kudos

Save ADC Data in Flash

Posted on July 26, 2013 at 09:54Hi,    I'm trying to sample a signal with the ADC and store data in the Micro Internal Flash.    At the moment I sample the data with the ADC in continous mode and save the Data from ADC1_DR_Address with the DMA in RA...

STM32f100R8-USART1 Configuration

Posted on July 24, 2013 at 09:24Hi All,          Basically i want to configure the USART1 in the STM32f100R8 uC. The following code i have written for configureing USART1. //UART1 initializationRCC->APB2ENR |= RCC_APB2ENR_AFIOEN + RCC_APB2ENR_IOPAEN...

dharani by Associate II
  • 2613 Views
  • 5 replies
  • 0 kudos

STM32F2xx Keil Performance Analyzer

Posted on July 25, 2013 at 19:17Hi all,I am using the STM32F207IG with uVision4 from Keil.For my suprise, the perfomance analyzer didnt apear in the Debug Section.I have found this link that show how to active: ''http://www.keil.com/support/man/docs...

felipe by Associate II
  • 2039 Views
  • 3 replies
  • 0 kudos

STM32L152RB EEPROM Confusion

Posted on July 25, 2013 at 17:24I have a couple questions about the onboard eeprom found in the STM32L152RB and similar devices.  My first question has to do with erasing the memory.  CD00242299 (the flash programming application note) mentions a d...

kevin by Associate II
  • 1092 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.