STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F373C8 Minimal Schematic Design

Posted on July 05, 2013 at 18:08I looked around on this site and online, and I haven't been able to find a description of the basic circuit design that I need around the board for full functionality.  Does anyone know where i could find this, or wha...

mattfox by Associate II
  • 1392 Views
  • 2 replies
  • 0 kudos

stm32f4 discovery st-link usb problem

Posted on May 30, 2013 at 00:14i have problem with st link swd in discovery board. the usb device have problem in this picture. i think it need usb driver for discovery baord.

0690X00000605PpQAI.png
jbl_raw by Associate II
  • 2142 Views
  • 4 replies
  • 0 kudos

STM32F205: DMA2 operation with ADC1 problem

Posted on July 29, 2013 at 17:54 Hello, I have a problem to work the DMA2 with ADC1 on STM32F205 chip. Problem is the interrupt routineDMA2_Stream0_IRQHandler is never executed despite of configuration is performed. The flag TCIF0 is howe...

clement2 by Associate
  • 1755 Views
  • 2 replies
  • 0 kudos

EXTI doesn't wake up STM32L from Stop Mode

Posted on July 02, 2013 at 08:32Hi all, I am trying low power modes on STM32L151C6, but when I give the following lines, no interrupts seems to be able to wake up the MCU from Stop Mode. From manual: ''Mode exit: (WFI) Any EXTI Line configured in I...

STM32F407 RTC timestampping

Posted on July 25, 2013 at 11:06Hi All,I wanted to timestamp external events with a resolution of 10's of milliseconds. How can I do that in STM32F407 ?Best Regards,K #rtc

khalid by Associate II
  • 2392 Views
  • 4 replies
  • 0 kudos

stm32 and accumulator

Posted on July 29, 2013 at 14:24I have a question, I'm doing the robot. Is it possible to feed the controller from the battery and usb or is it dangerous?

svarog995 by Associate II
  • 1140 Views
  • 1 replies
  • 0 kudos

Virtual COM Port CDC on STM32F4-Discovery

Posted on July 29, 2013 at 11:59Hi all,I try to implement a CDC Device on STM32F4-discovery.I made an IAR project based on the VCP example project of the STM32_USB-Host-Device_Lib_V2.1.0.The STM32-Discovery starts correctly but two ''STM32 Virtual C...

pfifre by Associate II
  • 607 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.