STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Array initialization

I know that the question will be trivial, however, I do not understand why the instruction uint8_t dataRx[4] = { 1 }; does not initialize all the elements of an array to 0 ... but only the first one:I have programmed little in the last while so I wil...

stm32 array 2.png
luke514 by Senior
  • 2481 Views
  • 2 replies
  • 5 kudos

SPI communication (Receive Only Master)

We are trying to develop a device that uses SPI communication (Receive Only Master).Are there any sample programs for SPI communication (Receive Only Master)?Which should be executed first: "Receive Only Master HAL_SPI_Receive" or "Transmit Only Slav...

STM32L0 STOP and STANDBY mode.

I have some questions. I read that STOP mode has a "RAM retention", so when it wakes up it the whole data is still intact (not cleared).When the RAM retention is off then the data is gone when it goes to STOP mode. So when it Wakes up does it restart...

Xenon02 by Senior
  • 10055 Views
  • 13 replies
  • 4 kudos

STM32H7B0 How to get input frequency of timer 3

Dear,Used MCU: STM32H7B0, 100 pins.In the datasheets we had found that TIM3 use the APB1 peripheral clock.In our case is this 120MHz. But when we use the function "HAL_RCC_GetPCLK1Freq()" we become 60MHz.This isn't correct. So what function should we...

OGhis_0-1730552934505.png
OGhis by Senior
  • 2076 Views
  • 4 replies
  • 1 kudos

Resolved! STM32H7B0 ADC 2 incorrect sample rate.

Dear,Using STM32H0B0, 100 pins version.we wish to sample 1 input with ADC2 at a fixed frequency. This must not deviate and for this we use timer 3 set to the desired sample rate.In the pictures we use 100Khz, but later to go to 1Msps.So the timer 3 i...

OGhis_3-1730578411629.png OGhis_0-1730577254510.png OGhis_1-1730577267859.png OGhis_2-1730577285068.png
OGhis by Senior
  • 1968 Views
  • 1 replies
  • 0 kudos

STM32 SPI master and slave issue

Hello everyone.I am working on a project and I have two stm32 MCU connected over SPI interface. One acting as a master (STM32H743VIT6) and the second acting as a slave (STM32C011U6) in full duplex.When sending data between the two devices the receive...

sousa_1-1730544656409.png
sousa by Associate II
  • 2435 Views
  • 5 replies
  • 0 kudos

Unexpected timing with nops

Hi,I am confused with pin toggle timings, why I am getting non equal pulse widths like in the picture, I turn off all compiler optimizations and disable all of the interrupts, code is simple pin toggling. My controller is STM32L431 running on 80MHz.T...

pic2.png
tompa by Associate III
  • 5934 Views
  • 14 replies
  • 8 kudos

Resolved! High AD noise on STM32F103 (bluepill)

This is on STM32F103C8 (bluepill)The A0 is connected to a voltage divider between bluepill's 3v3 and GND,And the output is very noisy. adding a delay did't do not much good```void setup(){Serial.begin(9600);// Enable ADC1 and configure itRCC->APB2ENR...

pilot by Associate III
  • 1616 Views
  • 2 replies
  • 1 kudos

stm32h755 Nucleo M7 debug problem

I am Juan de Jesus, I am a graduate student in engineering. I just bought a NUCLEO STM32H755 board.I am writing a simple code to test this board, an algorithm that makes LED 1 blink.The program compiles very well, and after this, I have made the conf...

SDIO Bit Start Error with STM32F407VGT6 and STM32CubeMX

Posted on January 11, 2015 at 20:46I'm having problems with communication through SDIO. In the initialization process, where are only sent commands, everything works, but the function HAL_SD_SendSDStatus is returning SD_START_BIT_ERR. Informations a...

silas by Associate II
  • 2112 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.