STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error stm32G030 not specified in the errata file.

When using RTC, the GPIO pin state of PA4 may be corrupted. RM0454, section 23.3.3 says: "In addition, it is possible to output RTC_OUT2 on PA4 pin thanks to OUT2EN bit. Thisoutput is not available in VBAT mode. The different functions are mapped on ...

PBobo.1 by Associate II
  • 6052 Views
  • 11 replies
  • 1 kudos

Resolved! STM32F756 jumps unknown address "BX LR"

Hello everyone,I and my collegue have more than 20 years experience on embedded desing with MCUs. We have a problem which we haven't seen this kind of problem before. I guess someone can help us in here.MCU: STM32F756IDE: Project created from cubeMX ...

1.png 2.png 3.png 4.png
MuratUnal by Associate II
  • 2375 Views
  • 4 replies
  • 2 kudos

Resolved! wrong value for FMODE in RM 0433

The reference manual 0433 Rev 8, p. 900, section 23.5.5 says "This bitfield has no effect when in memory-mapped mode (FMODE = 10)." But p. 901, section 23.5.6 says: "11: Memory-mapped mode".Could someone please let the authors fix this?Thank you.

HRTIM: won't trigger regular channel ADC

Hi,I'm using STM32G474 to drive my BLDC motor, i want to trig low-side phase current sensing ADC when the lower MOSFET is conducted. But the wired thing is even though CMP2 callback did be called by interrupt, ADC also not triggered (ConvCpltCallback...

Resolved! STM32H503RB I3C dynamic address assignment for sensors

Hi Foued,I'm going to connect 10 BMI323 IMUs to STM32H503RB MCU by I3C bus. BEI323 supports I3C and dynamic addressing and 0x68 static address. Is it possible for I3C bus of STM32 to recognize all IMUs by assign different I3C addresses to make all of...

kaosun by Associate II
  • 1656 Views
  • 1 replies
  • 0 kudos

Resolved! OCTOSPI interface for communication with a FPGA

Hi AllI have created a PCB where I want to use the OCTOSPI to communicate with a FPGA.I have difficulty finding accurate information on how the different memory types work. I already have a Hyperram running so I started there, that did also seem stra...

Kvang_2-1723555880449.png Kvang_1-1723555699939.png Kvang_0-1723555242998.png
Kvang by Associate III
  • 5468 Views
  • 8 replies
  • 3 kudos

IWDG findings

[This is a reconstruction of a thread I've started on Mar 26, 2017, but got lost in the two forum software transitions since then.]Reports in IWDG short period (125 us) problem  and STM32F407 : IWDG and erase flash sector  indicate that the IWDG does...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.