STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI need help

Posted on July 16, 2013 at 05:15 So ive been trying to get the SPI interface working. Here's what i have so far. void SPI_Setup(void) { SPI_InitTypeDef SPI_InitStructure; SPI_I2S_DeInit(SPI1); SPI_InitStructure.SPI_Direction = SPI_Dir...

timothy by Associate II
  • 1655 Views
  • 4 replies
  • 0 kudos

need STM32F0 SPI Slave Tutorial / working example

Posted on August 08, 2013 at 19:23hi all.. i'm already searching for hours, and can not find a working example / tutorial for SPI Slave on STM32F0. Anyone ?thanks before... #need-stm32f0-spi-slave-tutorial

septijo by Associate II
  • 1994 Views
  • 4 replies
  • 0 kudos

Fatal error: Can not connect to J-Link via USB. Session aborted!

Posted on August 07, 2013 at 23:41I have a STM32 Discovery Kit.  I have set up the IAR compiler.  Succesfully compiled code.  However when I try to download the the Discovery Board I get the following message... Wed Aug 07, 2013 14:21:48: Fatal erro...

greg by Associate II
  • 3098 Views
  • 5 replies
  • 0 kudos

STM32F103VET6 ,converts RGB/YCrCb image data to JPEG

Posted on August 07, 2013 at 10:12Can you help me a little bit?My thesis is about writing the code for image compression and decompression on STM32F103VET6. I have a RGB file and my tasks are writing 1 code to convert the RGB to a JPEG and writing 1...

amore by Associate II
  • 2650 Views
  • 4 replies
  • 0 kudos

STM32F4 Discovery + DM-STF4BB + 180 deg.

Posted on August 08, 2013 at 16:42Hi,I've bought those two boards, but for about 20s DM-STF4BB was rotated 180 deg. so +5V and +3V3 goes somewhere where shouldn't. Do you think DM-STF4BB survived?Second question: from where I can download examples f...

zenek by Associate
  • 1939 Views
  • 3 replies
  • 0 kudos

I2C busy flag

Posted on August 05, 2013 at 12:10 Hello, I am trying to connect two boards using I2C. I have already configured one as master but whenever I send the start condition the I2C bus is busy. Maybe I am wrong in the initialization of the GPIO...

edgar by Associate II
  • 2234 Views
  • 4 replies
  • 0 kudos

NVIC - Defining software interrupt

Posted on August 08, 2013 at 08:37 Hi , I want to add a new interrupt to the system , i know that the NVIC can support up to 256 interrupts , currently in my evaluation boad ( stm32f4g-eval) there are only 81 used . So i added a new on...

Why is DMA reducing my pulse width?

Posted on August 01, 2013 at 03:43Howdy,     So I enabled DMA1, on STM32F103, copying two 32-bit words (set and clear PF.15) from flash to GPIOF->BSRR at 25kHz.  I then run this code with all interrupts disabled while(1) {     GPIOF->BSRR = 1 << 14;...

bikejog by Associate II
  • 8407 Views
  • 20 replies
  • 0 kudos

STM32F4 Free running 32-bit timer/counter

Posted on August 07, 2013 at 20:14Can someone please point me in the right direction to use TIM2 or TIM5 as just a free running 32-bit counter, ticking at 1us, that I can read anywhere in my pgm.  No I/O or interrupts desired. None of the examples i...

USART NOT receiving nothing

Posted on August 07, 2013 at 07:12Im using usart2 and i know its sending data but will not receive im using :rx_data = USART_ReceiveData(USART2);to save the data then using a while(rx_data > 0 ) { do stuff}any suggestions about why its not receiving...

timothy by Associate II
  • 3495 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.