2013-08-09 11:11 AM
I'm working with the STM32F3 Discovery board. I'm wondering if it is possible to use a timer in encoder interface mode with the signals coming in on Channels 1 and 4. Do you have to use channels 1 and 2? Does the Timer just measure the difference between the two channels that are initialized? Thanks for the help in advance!
2013-08-09 12:00 PM
I've solved my problem, even if I'm not too sure of the answer to this question. I don't think that it's possible from what I read online, but I figured out a way to use channels 1 and 2 on a different bus for my implementation.
2013-08-11 4:11 PM
Typically it pairs TI1 and TI2 for the encoder, I'm not sure you can use it with other pairings like 3/4.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.