STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32f407 DIsovery ADC Issue

Posted on October 16, 2013 at 15:00Hi, I have a relay circuit which has fourteen relay output (i.e 14 devices can be switched on or off from this) , I have attached the circuit for a single output. I am sending command to switch on the related outp...

STM32F4Discovery - I2S config

Posted on July 22, 2013 at 18:28 Hi all! I'm new in forum. I wrote this config for I2S. Instead of MCLK=256*Fs=12, 288000 MHz and CK=48KHz*32bit*2channel=3, 072000 MHz, I measured MCLK=4MHz and CK=1 MHz. My code is: ...

uprogc by Associate II
  • 2532 Views
  • 6 replies
  • 0 kudos

Software interrupt doesn't work - please help

Posted on September 09, 2013 at 17:04Hi, I try to set a software interrupt. I set it as follows: &sharpdefine HZ500_EXT_INT_LINE                                EXTI_Line1 &sharpdefine HZ500_EXT_INT_IRQ                                    EXTI1_IRQn &...

igal by Associate II
  • 1882 Views
  • 4 replies
  • 0 kudos

USB device : re-connect after a reset

Posted on March 15, 2013 at 09:28Hello everybody, I have a question about USB device in VCP mode. I would like to keep my VCP communication open after a microcontroller reset (STM32F207). Is it possible ? In example, I have a terminal software runni...

Audio Synthesizer

Posted on October 16, 2013 at 01:45Hey guys,I've recently been designing a synthesizer based on the STM32F4 Discovery board. I'm using a PT8211 DAC for the audio output and an interrupt triggered at 48KHz. My audio is generated using a DDS method an...

harris by Associate II
  • 814 Views
  • 0 replies
  • 0 kudos

STM32F103VCT6 as a CSI (camera) reader

Posted on October 14, 2013 at 20:54hi i am in the middle of an R&D phase setting up a tablet where audio and camera will be controlled by an STM32F as a general-purpose peripheral (status is here: http://rhombus-tech.net/community_ideas/kde_tablet/n...

lkcl by Associate II
  • 1173 Views
  • 2 replies
  • 0 kudos

SD file to LCD

Posted on October 14, 2013 at 18:51JPG To SD I'm an absolutely beginner in microcontrollers. I want to display jpg from SD Card. I  create a list file from sd card, but I have no idea for next step Can anybody tell me the next step? Thank You Photo...

stm3223 by Associate II
  • 2017 Views
  • 4 replies
  • 0 kudos

How to detect infinite loop in program flow

Posted on October 14, 2013 at 19:48Hi ALL , I have a question that is bugging me lately and i could not find any good solution for the problem. Suppose I have a function , that may or may not , depend on the input and the amount of fixed bugs ;) , ...

RTC reference clock detection

Posted on October 15, 2013 at 14:44Hello,we want to build a system with some STM32F407s. For error memory, it is important that all controllers have the same time. I would like to use the RTC and the RTC_REFIN input to synchronize the RTCs.The RTC w...

STM32L152xD: SPI+DMA transfer with IO trigger

Posted on October 14, 2013 at 15:49I'm new to STM32 so please help :) Is that possible to trigger SPI+DMA transfer from GPIO? I have RM0038 document and on ''DMA1 request mapping'' (page 213) diagram there are no GPIO pins. I assume that SPIx_RX and...

keebler by Associate
  • 1408 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.