STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

migrating STM32L152VB to STM32L152VC/STM32L152VD

Posted on August 30, 2013 at 14:35Hello,I'd like to change the current STM32L152VB (LQFP100) to the bigger xC or xD. Are there any differences in terms of pinout and/or software? Is there any migrating application note?Thanks and best regards

bruzzim by Associate II
  • 1621 Views
  • 2 replies
  • 0 kudos

bsdl for SMT32L151XX

Posted on October 16, 2013 at 05:01I can not find BSDL file of Med-density Ultra-low for STM32L151xx and STM32L152xx microcontrollers as described in readme.txt. #smt32l151 #ask-smarter-questions

STM32F407 external frequency counting

Posted on October 16, 2013 at 11:17Hello folks, i have to try write a C-Code for counting an external frequency in a Range of 250ms. I tried to use the encoder mode, but i think it is impossible only with one signal. In my project i have only one fr...

STM32F3Discovery clock and sleeping issues

Posted on October 16, 2013 at 10:11 Hello everyone! Now I'm playing with STM32F3Discovery which has STM32F303 on the board. The goal for this MCU is typical: do some gpio stuff -> sleep for a while (STOP mode) -> wake up -> gpio. There i...

STM32L152RB Timer Interrupts

Posted on October 16, 2013 at 23:08 I've been trying to solve this issue for way too long now. I've looked at other similar posts, but I am still unable to enter my ISR when the timer rolls over. void init_interface(void) { GPIO_InitT...

kevin by Associate II
  • 2008 Views
  • 3 replies
  • 0 kudos

Problems using FPU and GCC on STM32F3

Posted on October 16, 2013 at 20:18 Hello, I'm currently working on a motor application where i need to perform some simple math but at a high rate (20khz). Unfortunately, for some reason the computation time is too long, and it is unable...

STM32F205 ULPI

Posted on October 16, 2013 at 11:55Has anybody here gotten the STM32F205 ULPI HS USB to work with SMSC USB3317?. or for that matter any of the SMSC USB transceivers? Thanks,

ramv by Associate II
  • 1827 Views
  • 3 replies
  • 0 kudos

stm32f107vc - external interrupt problem

Posted on October 16, 2013 at 00:21hello forum . I am trying to use external interrupt but I can't do it and I can't understand what is wrong. here is my code :#include ''stm32f10x.h''#include ''stm32_eval.h''#include <stdio.h>GPIO_InitTypeDef gpio_...

How to use bootloader to upgrade bootloader in STM32?

Posted on October 14, 2013 at 10:11I designed a bootloader and erase it to sector 0. It can erase other bin into other sectors using IAP. But how to  upgrade itself to sector 0? Does anyone give me an idea? Thanks.

ray by Associate II
  • 1837 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.