2013-10-14 11:54 AM
hi i am in the middle of an R&D phase setting up a tablet where audio and camera will be controlled by an STM32F as a general-purpose peripheral (status is here: http://rhombus-tech.net/community_ideas/kde_tablet/news/)
before going for a 3rd revision of the PCB i'd very much appreciate some guidance on how to do this properly. the original software i planned the schematics around does bit-banging in an ISR (https://github.com/adamgreig/followingrobot) as the STM32F103VCT6 needs to do other tasks, 100% CPU load reading the camera data isn't acceptable! so i have looked around and learned that it may be possible to read up to 6mhz of GPIO via DMA. the problem i have is that it's an external pixel clock coming from the camera. what i've done so far: * confirmed with a scope that the camera runs (at 12mhz) by directing HSE to PA8 as a MCO * confirmed that the camera is then contactable over I2C (it is) * initialised it (successfully) * asked it to set its Pixel Clock to 6mhz (also successful) note here that whilst there is a master-clock in to the camera, the camera then has an *output* (called Pixel Clock) which, obviously, syncs the 8 (or 10) bits of data out. there's also an HSYNC and a VSYNC output: these are also connected up to GPIO lines. the next phase is, clearly, to read the data. here is the plan that i believe is necessary: * connect the camera's Pixel Clock line to e.g. PE0/TIM4_ETR * set DMA2 to sync to TIM4 * set up DMA2 to do memory-to-memory transfer from PD8-15 * have EINT connect to the camera HSYNC line which starts DMA the rest i can deal with (USB transfer of the data) but i wanted to get people's opinions on whether this looks like a viable plan. i'm well aware that the STM32F207VCT6 already has DCMI but the project is cost-sensitive: although it would be nice to be capable of doing 720p24 using the STM32F207, we have to do 320x240 using a chip that's almost half the cost, first! so - is there anything unreasonable about this plan to connect ETR to Timer to DMA to PD8-15 to USB? :) thanks in advance for any guidance. l.2013-10-15 2:35 AM
* set up DMA2 to do memory-to-memory transfer from PD8-15
mem2mem won't work it should be peripheral to mem.IMO the whole setup might work if you are lucky, worth trying.
2013-10-15 2:21 PM
knik, hi, yes well spotted - in cut/paste of some code which does adc dma reading i noticed that one - thank you for confirming i'm on the right track!
i'm currently attempting just plain timer-controlled dma gpio reading: the next phase will be to do timer-externally-triggered.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.